MKM Internal Xtal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKM Internal Xtal

1,491件の閲覧回数
dhruvonline
Contributor III

Hi,

I need to configure the MKM UART with the Internal clock. The given driver files are with the external clock. I need to test the UART communication at standard baud rate with internal Clock.

Looking for the valuable suggestions for the same.

Thanks,

Druv

0 件の賞賛
返信
2 返答(返信)

1,385件の閲覧回数
dhruvonline
Contributor III

Hi Martin,

I am able to get the UART data with this example. Thanks for the support.

Thanks&Regards

Druv

0 件の賞賛
返信

1,385件の閲覧回数
MarMi
NXP Employee
NXP Employee

Hi Druv,

use any existing UART configuration structure but provide exact frequency in Hz, generated by internal clock, as the clk parameter into structure - see below:

UART_MODULE_POLLMODE_CONFIG(brate,clk)

Refer to the afelp_test example for more details in how to run UART clocked by FLL configured in Bypassed Low Power Internal 2 MHz (BLPI) mode.

Kind regards,

Martin M.