MKL25Z32VFM4 IC not working properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL25Z32VFM4 IC not working properly

1,319 Views
prakasknair
Contributor I

I am using a MKL25Z32VFM4 IC which is in 32 pin QFN package on PCB designed for my project.

The problem is that, i am getting 1 Volt on VOUT33 pin (no 5) and reset pin (no. 19), whereas I should be getting 3.3 Volts on both.

I have already connected a pull up of 10k on reset pin,

checked the VDD and VSS and they are perfect.

I request all to suggest me the possible cause for this behavior and the remedy

0 Kudos
Reply
1 Reply

1,236 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Prakask,

I'd like to know whether you had already programed the application code to the MCU or not.

If it's ok, I'll appreciate when you can share the SCH of the mini-system.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply