MKL17Z64VFM4 MCU,Why do enter BOOT ROOM endless loop?I should how to set FOPT for to run my application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL17Z64VFM4 MCU,Why do enter BOOT ROOM endless loop?I should how to set FOPT for to run my application

2,285 Views
thoomanwang
Contributor V

I use a MKL17Z64VFM MCU,when i run debug, system enter BOOT ROOM mode,and it is a endless loop,Should i how to set FOPT ?

I hava try to many combination,But result is same.

pastedImage_1.png

pastedImage_2.png

Labels (1)
0 Kudos
Reply
2 Replies

2,167 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please read "13.3.3 Start-up Process" of KL17P64M48SF2RM and then check these conditions:

force the hardware to start the Kinetis Bootloader.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,167 Views
thoomanwang
Contributor V

because the board is my manual solder,i do not find a tin ball link NMI to gnd

Thanks

Thooman

0 Kudos
Reply