MKL04Z16 - SWD_CLK as Output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKL04Z16 - SWD_CLK as Output

1,508件の閲覧回数
juergene
Contributor III

Hello community,

i have a design with a MKL04Z16 controller and we want to use the Pin 30 (SWD_CLK in default) as GPIO Output. 

It is possible to use this as output (see screenshot)pastedImage_1.png

But is it possible after flashing the SWD_CLK as output to debug again ?

Thanks in advance.

Best regards,

Juergen

ラベル(1)
0 件の賞賛
返信
1 返信

1,401件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Juergen,

This pin can be configured as GPIO Output.
But it's not recommended due to it will effect SWD function when you want to debug it again.
You may need to recover it by specify method: Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信