MKL02 programming problem after reset disable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKL02 programming problem after reset disable

4,019 次查看
OilCastle
Contributor III

Hello, I`m newbie.

my target is MKL02 (FRDM-KL02Z board)

my problem is this

i`m checking reset pin change to gpio, and i did it.

and i mistake is every pin (include SWD pin) setting as gpio

and now i cannot program on my target

i`m using Keil uVision

anyone dose know how to program in this case?

if you know, plz, give me hint (like datasheet or ref. manual page)

now i`m little-bit panic, so i`ll take some coffee

have a nice day.

5 回复数

3,798 次查看
OilCastle
Contributor III

thanks for your help pavel

i already change my MCU.

before i tried full chip erase, MCU dose not connect with openSDA j-link

after this if i have chance, i`ll try your way

have a nice day

and thanks

0 项奖励
回复

3,798 次查看
pavel_krenek
NXP Employee
NXP Employee

Hi,

I attached script for flash unsecuring using j-link. You can try to by this method, if you aren't lucky you need to change the MCU. Pls unzip the file and try to start unsecure.bat.

Regard,
Pavel

3,797 次查看
pavel_krenek
NXP Employee
NXP Employee

Hi Jun,

do mass erase of the flash memory. I hope you can do it in Keil or if not you can use some external tool.

BTW what type of debug tool are you using ?

Best regards,

Pavel

0 项奖励
回复

3,797 次查看
OilCastle
Contributor III

well, it`s not working.

i disable reset pin by startup code

and after reset, SWD pin is set as a gpio (i messed up)

i tried open SDA j-link for full-chip erase

but it is not connected with j-link

should i change  my chip?

or there are any other way i don`t know?

have a nice day.

0 项奖励
回复

3,797 次查看
OilCastle
Contributor III

thx for answer pavel.

i`m using openSDA on KL02Z board

and now i`ll try Multilink Universal

i wish it works

0 项奖励
回复