MKE16Z64 mcu xpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKE16Z64 mcu xpresso

1,525件の閲覧回数
ravindra
Contributor I

Hi

 

i am working on kinetic mcu MKE16Z64VLF4 by using mcu xpresso ide,but i have some project which in written in code warrior. the concern is i want to import the code from code warrior to mcuxpresso because of limited timeline.please share if we have some solution for the same.

0 件の賞賛
返信
1 返信

1,517件の閲覧回数
mjbcswitzerland
Specialist V

Hi

If your code warrior project builds with GCC it is simple to move to MCUXpresso (or between KDS, Atollic, or other Eclipse based IDEs). You just need to configure the settings again (they can't be imported since the IDE project configurations are not compatible) - to do this open the original Code warrior project and the new workspace at the same time and copy each of the settings (like pre-processor defines, include paths, processor type) and then it tends to already work.

 

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements

For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key

 

0 件の賞賛
返信