MKE15Z256VLL7 with strange marking that has programming problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKE15Z256VLL7 with strange marking that has programming problems

2,352件の閲覧回数
MarcoAEE
Contributor II

Hi,

I have a production batch with MKE15Z256VLL7 MCUs that have a strange marking, there is one more line than usual with the following writing: QUAL3NN (I attach a photo)

MCU wrong marking.jpg


I cannot program or delete them in any way with JLink, I attach a log. They are not blocked and in any case J-Link Command cannot execute the "unlock kinetis" procedure.

JLinkLog.jpg

UnlockFaild.jpg
If I replace the MCU with one with a normal marking, everything works normally (I attach a photo of the "normal" MCU)

MCU correct marking.jpg


Has anything similar ever happened to anyone?


Thanks
Marco

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,324件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @MarcoAEE ,

Thanks for contacting us.  I have never seen such a mark before. Just to confirm, was this chip obtained from NXP's official channels, such as the NXP official website or an authorized NXP distributor?

BRs,

Celeste

0 件の賞賛
返信

2,317件の閲覧回数
MarcoAEE
Contributor II

Hi @Celeste_Liu,

unfortunately this is information that I don't have with precision.

The project is mine and I have already made other production batches. As for the other batches we relied on a well-known Chinese supplier of PCB and PCBA, through which we purchased the components.
Obviously I also asked them for explanations on the origins of the component and I am waiting for an answer.

However, assuming that it is a fake IC, it seems strange to me that during the connection phase with JLink the component responds correctly. What do you think?
Are there any commands to get more information (type identifier, production batch, etc...)?

Thanks
Marco

0 件の賞賛
返信

2,297件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @MarcoAEE ,

Thanks for your reply.

For your question: Are there any commands to get more information (type identifier, production batch, etc...)?

-> No commands. 

The production batch can be found in the third line of the chip mask. For example, the batch number of this chip is "XNJH2226AM".

How many chips with an additional line do you have?
We need you to confirm the the origins first so that we can help you further. Thank you for your understanding.

BRs,

Celeste

0 件の賞賛
返信

2,294件の閲覧回数
MarcoAEE
Contributor II

Hi @Celeste_Liu ,
thanks for the reply; I have 10 of them, all the same, with the same marking as the photo attached in the first message.
Can you confirm that the last line cannot possibly have been put by NXP?
Thanks
Marco

0 件の賞賛
返信

2,288件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @MarcoAEE ,

I have created a private case for you. You can contact me through that. Please check your email inbox.

BRs,

Celeste

0 件の賞賛
返信