MKE15Z256VLH have GPIO interruption?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKE15Z256VLH have GPIO interruption?

ソリューションへジャンプ
1,630件の閲覧回数
Jmir
Contributor II

I plan on coming to adopt the MKE15Z256VLH7 ( KE1xZ serie) in a new project due to its expected longevity.

From the analysis of the datasheet I find no reference to interruptions by GPIO. I will have a  input of pulses from an encoder that will have to be treated by interruption to calculate speed.Someone confirm me if this chip has interruptions by GPIO?

0 件の賞賛
返信
1 解決策
1,610件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The pin interrupt is described in chapter 34.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,611件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The pin interrupt is described in chapter 34.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,624件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The KE1xZ and KE1xF parts have both port driven IRQ and DMA capabilities.
It is only the simple KE and KEA series that have only a single IRQ pin for interrupts.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements

For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key: https://www.utasker.com/kinetis/FRDM-KE15Z.html

0 件の賞賛
返信