MKE06Z64 connection error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKE06Z64 connection error

2,698 Views
karate_man
Contributor II

Hello

I made a target board for MKE06Z64VLD4.

First,  I set new empty project by CW10.6.  And  I pushed  debug button. But It appear loading error ARP......

I try to drive power 3.3V.  In this case, Target Connect is success from MultiLink universal.

But  Taget is not success 5V power.   I sure did install CW10.6 update 2.0.0 and updated Multilink debugger of P&E micro.

following connection message 3.3V and 5.0V

// -----------------------------------------------------3.3V----------------------------------------------------------------------------------------------------

Executing Initialization File: C:\Users\workspace\test3/Project_Settings/Debugger/init_kinetis.tcl

radix x

cmdwin::eclipse::config hexprefix 0x

cmdwin::eclipse::config MemIdentifier p

cmdwin::eclipse::config MemWidth 32

cmdwin::eclipse::config MemAccess 32

thread break: Stopped, 0x0, 0x0, cpuARMLittle, test3.elf (state, tid, pid, cpu, target)

cmdwin::eclipse::config MemSwap off

cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF

cmdwin::reg Breakpoint Unit Registers/BP_COMP0 = 0x0

cmdwin::reg Breakpoint Unit Registers/BP_COMP1 = 0x0

cmdwin::reg Core Debug Registers/DEMCR = 0x1000001

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALH = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALL = 0xE8

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS2 = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS1 = 0x23

Starting 3rd party flash programming...

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : 0, R) => DI_ERR_NONFATAL

INF: Copyright 2012 P&E Microcomputer Systems,Inc.

INF: Command Line :"C:\Freescale\CW MCU v10.6\eclipse\..\MCU\bin\de.exe" -noni -language en -ORBendPoint giop:tcp:127.0.0.1: -ORBtraceLevel 0

INF: CMD>RE

INF: Initializing.

INF: Target has been RESET and is active.

INF: CMD>CM C:\Freescale\CW MCU v10.6\MCU\bin\Plugins\support\arm\gdi\P&E\ke06z64m4_pflash_pipeline.arp

INF: Initializing.

INF: Initialized.

INF: ;version 1.02, 02/07/2014, Copyright P&E Microcomputer Systems, www.pemicro.com [ke_64k_pflash_ftmre_m0]

INF: ;device freescale, ke06z64m4, desc=pflash_pipeline

INF: ;begin_cs device=$00000000, length=$00010000, ram=$20000000

INF: Loading programming algorithm ...

INF: Done.

INF: CMD>EM

INF: Erasing.

INF: Module has been erased.

INF: Initializing.

INF: Initialized.

INF: ;version 1.02, 02/07/2014, Copyright P&E Microcomputer Systems, www.pemicro.com [ke_64k_pflash_ftmre_m0]

INF: ;device freescale, ke06z64m4, desc=pflash_pipeline

INF: ;begin_cs device=$00000000, length=$00010000, ram=$20000000

INF: Loading programming algorithm ...

INF: Done.

INF: CMD>PM

INF: Programming.

INF: Processing Object File Data ...

INF: .

INF: Programmed.

INF: CMD>VC

INF: Verifying object file CRC-16 to device ranges ...

INF:    block 00000000-000000BF ...

INF: Ok.

INF:    block 00000400-00000AFB ...

INF: Ok.

INF:    Checksum Verification Successful. (Cumulative CRC-16=$6A7D)

INF: CMD>RE

INF: Initializing.

INF: Target has been RESET and is active.

Executing download task: C:\Users\workspace\test3/Project_Settings/Debugger/init_kinetis.tcl

radix x

cmdwin::eclipse::config hexprefix 0x

cmdwin::eclipse::config MemIdentifier p

cmdwin::eclipse::config MemWidth 32

cmdwin::eclipse::config MemAccess 32

cmdwin::eclipse::config MemSwap off

cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF

cmdwin::reg Breakpoint Unit Registers/BP_COMP0 = 0x0

cmdwin::reg Breakpoint Unit Registers/BP_COMP1 = 0x0

cmdwin::reg Core Debug Registers/DEMCR = 0x1000001

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALH = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALL = 0xE8

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS2 = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS1 = 0x23

// -----------------------------------------------------5.0V----------------------------------------------------------------------------------------------------

Executing Initialization File: C:\Users\workspace\test3/Project_Settings/Debugger/init_kinetis.tcl

radix x

cmdwin::eclipse::config hexprefix 0x

cmdwin::eclipse::config MemIdentifier p

cmdwin::eclipse::config MemWidth 32

cmdwin::eclipse::config MemAccess 32

thread break: Stopped, 0x0, 0x0, cpuARMLittle, test3.elf (state, tid, pid, cpu, target)

cmdwin::eclipse::config MemSwap off

cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF

cmdwin::reg Breakpoint Unit Registers/BP_COMP0 = 0x0

cmdwin::reg Breakpoint Unit Registers/BP_COMP1 = 0x0

cmdwin::reg Core Debug Registers/DEMCR = 0x1000001

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALH = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALL = 0xE8

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS2 = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS1 = 0x23

Starting 3rd party flash programming...

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : 0, R) => DI_ERR_NONFATAL

INF: Copyright 2012 P&E Microcomputer Systems,Inc.

INF: Command Line :"C:\Freescale\CW MCU v10.6\eclipse\..\MCU\bin\de.exe" -noni -language en -ORBendPoint giop:tcp:127.0.0.1: -ORBtraceLevel 0

INF: CMD>RE

INF: Initializing.

INF: Target has been RESET and is active.

INF: CMD>CM C:\Freescale\CW MCU v10.6\MCU\bin\Plugins\support\arm\gdi\P&E\ke06z64m4_pflash_pipeline.arp

INF: Initializing.

INF: Initialized.

INF: ;version 1.02, 02/07/2014, Copyright P&E Microcomputer Systems, www.pemicro.com [ke_64k_pflash_ftmre_m0]

INF: ;device freescale, ke06z64m4, desc=pflash_pipeline

INF: ;begin_cs device=$00000000, length=$00010000, ram=$20000000

INF: Loading programming algorithm ...

INF: Done.

INF: CMD>EM

INF: Erasing.

INF: Module has been erased.

INF: Initializing.

INF: Initialized.

INF: ;version 1.02, 02/07/2014, Copyright P&E Microcomputer Systems, www.pemicro.com [ke_64k_pflash_ftmre_m0]

INF: ;device freescale, ke06z64m4, desc=pflash_pipeline

INF: ;begin_cs device=$00000000, length=$00010000, ram=$20000000

INF: Loading programming algorithm ...

INF: Done.

INF: CMD>PM

INF: Programming.

INF: Processing Object File Data ...

INF: .

INF: Programmed.

INF: CMD>VC

INF: Verifying object file CRC-16 to device ranges ...

INF:    block 00000000-000000BF ...

INF: Ok.

INF:    block 00000400-00000AFB ...

INF: Ok.

INF:    Checksum Verification Successful. (Cumulative CRC-16=$6A7D)

INF: CMD>RE

INF: Initializing.

INF: Target has been RESET and is active.

Executing download task: C:\Users\workspace\test3/Project_Settings/Debugger/init_kinetis.tcl

radix x

cmdwin::eclipse::config hexprefix 0x

cmdwin::eclipse::config MemIdentifier p

cmdwin::eclipse::config MemWidth 32

cmdwin::eclipse::config MemAccess 32

cmdwin::eclipse::config MemSwap off

cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF

cmdwin::reg Breakpoint Unit Registers/BP_COMP0 = 0x0

cmdwin::reg Breakpoint Unit Registers/BP_COMP1 = 0x0

cmdwin::reg Core Debug Registers/DEMCR = 0x1000001

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALH = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALL = 0xE8

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS2 = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS1 = 0x23

Executing Initialization File: C:\Users\workspace\test3/Project_Settings/Debugger/init_kinetis.tcl

radix x

cmdwin::eclipse::config hexprefix 0x

cmdwin::eclipse::config MemIdentifier p

cmdwin::eclipse::config MemWidth 32

cmdwin::eclipse::config MemAccess 32

thread break: Stopped, 0x0, 0x0, cpuARMLittle, test3.elf (state, tid, pid, cpu, target)

cmdwin::eclipse::config MemSwap off

cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF

cmdwin::reg Breakpoint Unit Registers/BP_COMP0 = 0x0

cmdwin::reg Breakpoint Unit Registers/BP_COMP1 = 0x0

cmdwin::reg Core Debug Registers/DEMCR = 0x1000001

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALH = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_TOVALL = 0xE8

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS2 = 0x03

cmdwin::reg Watchdog timer (WDOG)/WDOG_CS1 = 0x23

Starting 3rd party flash programming...

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : 0, R) => DI_ERR_NONFATAL

INF: Copyright 2012 P&E Microcomputer Systems,Inc.

INF: Command Line :"C:\Freescale\CW MCU v10.6\eclipse\..\MCU\bin\de.exe" -noni -language en -ORBendPoint giop:tcp:127.0.0.1: -ORBtraceLevel 0

INF: CMD>RE

INF: Initializing.

INF: Target has been RESET and is active.

INF: CMD>CM C:\Freescale\CW MCU v10.6\MCU\bin\Plugins\support\arm\gdi\P&E\ke06z64m4_pflash_pipeline.arp

INF: Initializing.

INF: Error loading .ARP file : C:\Freescale\CW MCU v10.6\MCU\bin\Plugins\support\arm\gdi\P&E\ke06z64m4_pflash_pipeline.arp. Set PC and Run Error.

ERR: Error loading programming algorithm - load aborted.

ERR: Error occured during Flash programming.

Please follow about this.

Labels (1)
0 Kudos
Reply
2 Replies

2,144 Views
karate_man
Contributor II

Hello, I've found the cause of this problem

PTB4 port is NMI signal of  default on MKE06Z64.

I connected this port to LED and resister to GND.

This NMI signal is read when the Reset signal rises.

At this time, NMI port is an internal pull-up. So ,this port cannot wire the pull down circuit.

And therefore, The voltage of NMI port drops in the influence of the LED&resister.

In 5.0V power supply, This voltage  decisioned low level for NMI state.

In 3.3V power supply, This voltage  decisioned high level for normal state.

If this signal is pulled down, CPU becomes NMI state.  This state is the same when the debugger conection.

thanks.

2,144 Views
capvdesign
Contributor II

Same problem same solution!!!

Thanks!

0 Kudos
Reply