MKE04Z8VFK4 (QFN 24) Production programming supplier

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKE04Z8VFK4 (QFN 24) Production programming supplier

2,566 Views
GeorgeChamberla
Contributor I

Hi,

Please recommend supplier who can production program Freescale  MKE04Z8VFK4  (QFN 24) Processors IC's.

First batch Qty 500.

Preferably without large NRE charge.

It appears Freescale/NXP no longer offer this service.

0 Kudos
Reply
4 Replies

2,394 Views
bobpaddock
Senior Contributor IV

Check with your distributor. 

They will often program the chips for you for a small price per chip.

This is the route we use here.

0 Kudos
Reply

2,394 Views
GeorgeChamberla
Contributor I

Hi Bob,

Thanks for your prompt reply.

I'm very interested to hear which didtributor provides your programing service.

0 Kudos
Reply

2,394 Views
bobpaddock
Senior Contributor IV

We use Arrow.  They are local to us and have reasonable per chip charge.

I'd look at the links that Ping posted to find one near you to work with rather than just using what we used.

0 Kudos
Reply

2,394 Views
jeremyzhou
NXP Employee
NXP Employee

Hi George,

I'd like to suggest you to contact with the local distributor through the link as below.

Distributor Network|NXP

Also you can bug the Cyclone MAX to do the programming which many customers prefers, you can go to bug it through the link as follow.

Cyclone MAX|NXP
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply