MK64 default output at reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK64 default output at reset

Jump to solution
2,095 Views
roymessinger
Contributor V

What is the default state of the outputs of the cobtroller immidiately after reset?

Do i need to put pull up/pull down on board?Regarding inputs, do i need to place pull up/pull down on inputs (or outputs) not used?

I've looked in the data sheet but probabely missed it.

Any help will do.

Thanks

0 Kudos
Reply
1 Solution
1,942 Views
egoodii
Senior Contributor III

The 'reset state' of all control registers is called out in the Reference Manual, including the 'pin mux' table, but the general statement is: 'reset state is the safest possible for any possible interconnect'.  That is, analog-in-capable pins will default to said analog-in mode, and digital pins will default to input, most with 'no pull'.

So yes, by-and-large anything you need to have as a 'known state' during/just-after reset will need your own external pull-resistors.

View solution in original post

0 Kudos
Reply
2 Replies
1,942 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Roy,

Some special function pins need take care. For exmaple: Reset_b\ NMI_b\ VREF_OUT\ JTAG_TMS

I recommend you read the "Chapter 2 General System Setup (Hardware Considerations)" of KQRUG.

General System Setup (Hardware Considerations).png

Best Regards,

Robin

0 Kudos
Reply
1,943 Views
egoodii
Senior Contributor III

The 'reset state' of all control registers is called out in the Reference Manual, including the 'pin mux' table, but the general statement is: 'reset state is the safest possible for any possible interconnect'.  That is, analog-in-capable pins will default to said analog-in mode, and digital pins will default to input, most with 'no pull'.

So yes, by-and-large anything you need to have as a 'known state' during/just-after reset will need your own external pull-resistors.

0 Kudos
Reply