MK64 FlexBus FB_RW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,355件の閲覧回数
DINGii
Contributor II

I'm using MK64, the FB_RW keeps being low after the write operation is finished, and the FB_RW returns high after the read operation, which seems to be 6800 mode, I need 8080 mode

0 件の賞賛
返信
1 解決策
2,324件の閲覧回数
DINGii
Contributor II

DINGii_0-1717192583689.png

The DM9000 write timing is shown in the figure, how does the MK64 FlexBUS implement it?

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,332件の閲覧回数
DINGii
Contributor II

DINGii_0-1717192140252.png

As you can see from the graph, the FB_RW stays low after the data is written

0 件の賞賛
返信
2,283件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

From the attached  FlexBus timing, it is incorrect, at least, the data bus should be valid until the rising edge of /CS signal.

Pls try different parameter in the FB_CSCRn register, especially, WRAH and WS bits, do not use burst mode, set AA bit in 1.

Pls have  a try.

BR

XiangJun Rong

 

0 件の賞賛
返信
2,340件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The Flex_Bus of K64 is in 8086 mode instead of 68K mode.

This is the reading timing:

xiangjun_rong_0-1717141109471.png

This is writing timing:

xiangjun_rong_1-1717141202761.png

Compare the two timing, you can see that the /FB_OE  low and the FB_RW high are observed in reading timing, the /FB_OE  high and the FB_RW low are observed in writing timing.

If the timing is 68K mode, the /FB_OE is always low no matter whether it is reading or writing.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信
2,325件の閲覧回数
DINGii
Contributor II

DINGii_0-1717192583689.png

The DM9000 write timing is shown in the figure, how does the MK64 FlexBUS implement it?

0 件の賞賛
返信
%3CLINGO-SUB%20id%3D%22lingo-sub-1878289%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EMK64%20%E3%83%95%E3%83%AC%E3%83%83%E3%82%AF%E3%82%B9%E3%83%90%E3%82%B9FB_RW%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1878289%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EMK64%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81%E6%9B%B8%E3%81%8D%E8%BE%BC%E3%81%BF%E6%93%8D%E4%BD%9C%E3%81%8C%E7%B5%82%E4%BA%86%E3%81%97%E3%81%9F%E5%BE%8C%E3%82%82FB_RW%E3%81%8C%E4%BD%8E%E3%81%8F%E3%81%AA%E3%82%8A%E7%B6%9A%E3%81%91%E3%80%81%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%8A%E6%93%8D%E4%BD%9C%E5%BE%8C%E3%81%ABFB_RW%E3%81%8C%E3%83%8F%E3%82%A4%E3%81%AB%E6%88%BB%E3%82%8A%E3%80%816800%E3%83%A2%E3%83%BC%E3%83%89%E3%81%AE%E3%82%88%E3%81%86%E3%81%A7%E3%81%99%E3%81%8C%E3%80%818080%E3%83%A2%E3%83%BC%E3%83%89%E3%81%8C%E5%BF%85%E8%A6%81%E3%81%A7%E3%81%99%3C%2FP%3E%3C%2FLINGO-BODY%3E