MK64 FlexBus FB_RW

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MK64 FlexBus FB_RW

跳至解决方案
2,347 次查看
DINGii
Contributor II

I'm using MK64, the FB_RW keeps being low after the write operation is finished, and the FB_RW returns high after the read operation, which seems to be 6800 mode, I need 8080 mode

0 项奖励
回复
1 解答
2,316 次查看
DINGii
Contributor II

DINGii_0-1717192583689.pngDINGii_0-1717192583689.png

The DM9000 write timing is shown in the figure, how does the MK64 FlexBUS implement it?

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,324 次查看
DINGii
Contributor II

DINGii_0-1717192140252.pngDINGii_0-1717192140252.png

As you can see from the graph, the FB_RW stays low after the data is written

0 项奖励
回复
2,275 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

From the attached  FlexBus timing, it is incorrect, at least, the data bus should be valid until the rising edge of /CS signal.

Pls try different parameter in the FB_CSCRn register, especially, WRAH and WS bits, do not use burst mode, set AA bit in 1.

Pls have  a try.

BR

XiangJun Rong

 

0 项奖励
回复
2,332 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The Flex_Bus of K64 is in 8086 mode instead of 68K mode.

This is the reading timing:

xiangjun_rong_0-1717141109471.pngxiangjun_rong_0-1717141109471.png

This is writing timing:

xiangjun_rong_1-1717141202761.pngxiangjun_rong_1-1717141202761.png

Compare the two timing, you can see that the /FB_OE  low and the FB_RW high are observed in reading timing, the /FB_OE  high and the FB_RW low are observed in writing timing.

If the timing is 68K mode, the /FB_OE is always low no matter whether it is reading or writing.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复
2,317 次查看
DINGii
Contributor II

DINGii_0-1717192583689.pngDINGii_0-1717192583689.png

The DM9000 write timing is shown in the figure, how does the MK64 FlexBUS implement it?

0 项奖励
回复
%3CLINGO-SUB%20id%3D%22lingo-sub-1878289%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EMK64%20FlexBus%20FB_RW%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1878289%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%E6%88%91%E7%94%A8%E7%9A%84%E6%98%AFMK64%EF%BC%8C%E5%86%99%E6%93%8D%E4%BD%9C%E5%AE%8C%E6%88%90%E5%90%8EFB_RW%E4%B8%80%E7%9B%B4%E4%B8%BA%E4%BD%8E%EF%BC%8C%E8%AF%BB%E6%93%8D%E4%BD%9C%E5%AE%8C%E6%88%90%E5%90%8EFB_RW%E5%8F%88%E6%81%A2%E5%A4%8D%E4%B8%BA%E9%AB%98%EF%BC%8C%E5%A5%BD%E5%83%8F%E6%98%AF6800%E6%A8%A1%E5%BC%8F%EF%BC%8C%E6%88%91%E9%9C%80%E8%A6%818080%E6%A8%A1%E5%BC%8F%3C%2FP%3E%3C%2FLINGO-BODY%3E