MK60F120M NFC virtual page

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60F120M NFC virtual page

2,689 Views
henrynguyen
Contributor IV

Hello,

I have used the MK60F120M eval board with the built in NFC + Nand device to do block erase, write page size = 2048 bytes and read page size = 2048 bytes with ECC enable.  Everything works fine.  No issue.  The catch is that the NAND device on MK60F120M eval board has 2048 byte physical page size.  It seems that it works well.

Now, i have another NAND device where the physical page size is 4096 bytes.  Physical number of block is 4096.  Physical number of pages per block is 128.  I configured the PEx as seen on the attachment below.  Immediately i noticed that the block count in Target description is 2048 which is a wrong value.  It should have been 4096 right?

now, when i ran the firmware to program and read back 4096 byte per page, sometimes, it worked correctly, sometimes, it had ECC error, sometimes, it did not read the second virtual pages, sometimes, there were few bytes flipped on the first virtual page.

my NFC clock is 1.5 MHz, that is way below the NFC clock the micron device is allowed.  

i also attached the NFC register dump on page write and page read as well as the generated codes from PE.

can you please advise me on what and how to configure the NFC correctly for the following device?

page size: 4096 bytes

spare space per page: 224 bytes

page count per block: 128 pages

block count per chip: 4096.

Does anyone has any example codes for MK60 interfacing to a physical page size larger than 2048 like 4096?

I have 8 Nand chips, so i do not use CE0 nor CE1.  I emulate CE0 / CE1 by toggling the GPIO for each NFC function.  

it seems that the timing is OK.

Thanks,

Henry

0 Kudos
Reply
2 Replies

2,577 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Henry,

Would you please specify which IDE tool you are using? Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,577 Views
henrynguyen
Contributor IV

Hi Kan,

i used KDS IDE 3.0 with SDK 1.3.

I think i have managed to get the Nand to work correctly for multiple Nands.  i have to use GPIO to select each Nand chip.

Still, i think there is a bug in PEx which it generates the block size of 2048 while i specify the block size of my device to be 4096.

Thanks,

Henry

0 Kudos
Reply