MK60DN512ZVLQ10 and FNET 2.1.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK60DN512ZVLQ10 and FNET 2.1.1

1,754件の閲覧回数
Arun_bel
Contributor I

I have created a project for MK60DN512ZVLQ10 using FNET 2.1.1 example shell demo application.

But the shell demo app is created for twr- mk60n512 board having MK60DN512VMD100 processor(BGA package).

So I have changed my processor settings and default UART settings.

Now UART is working fine but in Hyperterminal I am getting Link Status: unconnected .

Is there any changes to be done in any file if processor of same family I am using, particularly Pin change requirements.

Thanks and regards

Arun

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,610件の閲覧回数
tusharm
Contributor III

Hello Arun,

    

    Check the jumper connection i.e J2 and J3 u keep it for 50Mhz and J12 in RMII mode then execute your programs...If ur board is of 120Mhz i.e MK60F120M then use K70 example code...Or else better u down;load the latest FNET2.5...

Regards,

Tushar M

0 件の賞賛
返信

1,610件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Arun,

  Those packages (144 BGA and 144LQFP) will have the same pinout, so no pin changes are needed.

  Are you trying to run this code on a new custom board? Or are you just changing the software and still trying to run on a TWR-K60N512 board?

-Anthony

0 件の賞賛
返信