MK60DN512ZVLQ10 I2S RX issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK60DN512ZVLQ10 I2S RX issue

1,166 次查看
ganhongxing
Contributor I

I2S RX  master mode, 44.1k , but the MCLK, RX_BCLK, RX_FS are not output, no wave. the below is the configure. How can i do?

****************************************************************************/

void I2S_Init(void)

{

    SIM->SCGC5 |= SIM_SCGC5_PORTE_MASK;

    /* Enable SSI clock in SIM */

    // At first Disable system clock to the I2S module

    SIM->SCGC6 &= ~(SIM_SCGC6_I2S_MASK);

   

    SIM->SOPT2 |= SIM_SOPT2_I2SSRC(0);   //I2S clock source is system clock

   

    // divide clock source to I2S module to generate desired frequency

   

    // 48kHz

    //SIM_CLKDIV2 |= SIM_CLKDIV2_I2SDIV(7) | SIM_CLKDIV2_I2SFRAC(0);

   

    // Divide to get the 11.2896 MHz from 96MHz

    // for 44.1 kHz

    SIM->CLKDIV2 |= SIM_CLKDIV2_I2SDIV(16) | SIM_CLKDIV2_I2SFRAC(1);

   

    // enable system clock to the I2S module

    SIM->SCGC6 |= SIM_SCGC6_I2S_MASK;

    /* enable SSI pins */

    PORTE->PCR[6] = PORT_PCR_MUX(0x04);  // configure port for MCLK output

  

    //GPIO for SSI0_RX_BLCK

    PORTE->PCR[9] = PORT_PCR_MUX(0x04);  // 

    //GPIO for SSI0_RX_FS

    PORTE->PCR[8] = PORT_PCR_MUX(0x04);  //

    //GPIO for SSI0_RXD

    PORTE->PCR[7] = PORT_PCR_MUX(0x04);  // 

  

    /* Issue a SSI reset (bit 0 of I2S_CR */

    I2S0->CR &= ~I2S_CR_SSIEN_MASK;

   

    // initialize I2S Control Register (I2S_CR)

    // note reset values are all zero

    I2S0->CR =0

           | I2S_CR_I2SMODE(1)    // Set I2S master mode

         //| I2S_CR_I2SMODE(2)    // Set I2S slave mode

           | I2S_CR_SYSCLKEN_MASK    // Set clock out on SSI_MCLK pin

           | I2S_CR_SYN_MASK    // Enable synchronous mode

         //| I2S_CR_NET_MASK    // Enable network mode

           | I2S_CR_RE_MASK     // Enable the receive section, this does not enable interrupts

         //| I2S_CR_TE_MASK;     // Enable the transmit section, this does not enable interrupts

         //| I2S_CR_TCHEN_MASK  // Enable two channel mode

   ;

   

    I2S0->RCR = 0

          //| I2S_RCR_RXEXT_SHIFT 

          //| I2S_RCR_RXBIT0_SHIFT 

          //| I2S_RCR_RFEN1_SHIFT  // RX FIFO 1 enable

            | I2S_RCR_RFEN0_SHIFT  // RX FIFO 0 enable

            | I2S_RCR_RFDIR_SHIFT  

            | I2S_RCR_RXDIR_SHIFT

          //| I2S_RCR_RSHFD_SHIFT

            | I2S_RCR_RSCKP_SHIFT 

            | I2S_RCR_RFSI_SHIFT

   //| I2S_RCR_RFSL_SHIFT

   //| I2S_RCR_REFS_SHIFT

  ;

    I2S0->RCCR = 0

  | I2S_RCCR_WL(0x7)   // 16 bit word length

            | I2S_RCCR_DC(1)  // Frame rate divider

            | I2S_RCCR_PM(3);

              

   

    I2S0->FCSR = 0

            | I2S_FCSR_RFWM0(2)

            | I2S_FCSR_RFWM1(2)

            ;

   

    // initialize I2S Interrupt Enable Register (I2S_IER)  

    I2S0->IER =   0 /* interrupts */

              //| I2S_IER_TIE_MASK      /* turn on transmit interrupts */

              //| I2S_IER_TDE0EN_MASK   /* turn on transmit data 0 empty */

              //| I2S_IER_TDE1EN_MASK   /* turn on transmit data 1 empty */

              //| I2S_IER_TFE1EN_MASK   /* turn on transmit frame 1 empty */

              //| I2S_IER_TFE0EN_MASK   /* turn on transmit frame 0 empty */

              //| I2S_IER_RIE_MASK      /* turn on receive interrupts */

              //| I2S_IER_RDR0EN_MASK   /* turn on receive data 0 full */

              //| I2S_IER_RDR1EN_MASK   /* turn on receive data 1 full */

              //| I2S_IER_TDMAE_MASK    /* DMA request enabled */

   //| I2S_IER_RDMAE_MASK

               ;

    /* enable i2s */

    I2S0->CR |= I2S_CR_SSIEN_MASK;

   

}

标签 (1)
标记 (3)
0 项奖励
回复
0 回复数