MK60DN512VMD10 - Which Header File

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60DN512VMD10 - Which Header File

Jump to solution
2,215 Views
neillewis
Contributor II

I've just started programming with the Kinetis K60 MK60DN512VMD10 and have a problem with the differences between register definitions in the Reference Manual and the header files supplied with both Codewarrior and IAR compilers :-

"K60 Sub-Family Reference Manual" "Supports: MK60DN512VMD10" - (K60P144M100SF2V2RM Rev. 2 Jun 2012)

and

MK60N512VMD100.h

There are many detail differences but a good example is the MCG Registers.  These go up to MCG_C6 in the header file but go up to MCG_C10 in the Reference Manual.  Furthermore, many of the "bit mask" definitions in the header file don't have the "0" appended from the Reference Manual, eg, "MCG_C"_RANGE0" etc. Some even have completely different names..!

For now I'm building based on the example code provided by Freescale and I must use this header file because the register names match those in the various examples and in the "Kinetis Peripheral Module Quick Reference" (KQRUG, Rev. 0, 11/2010).

To get correctly named registers I would need to substitute the header file "MK60D10.h", but even that only goes up to MCG_C8... :-)

Since I don't want to be coding my project with incorrect register definitions, which is correct?

Perhaps these chips changed over time and I need the definitions for the correct age of chip?

Is there a header file which matches the registers in the Reference Manual?

Neil


Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,872 Views
neillewis
Contributor II

I did more research and happened upon this document describing the differences between Issue 1 and Issue 2 of the K60 100 MHz chips.  As far as I can tell the later 120 and 150 MHz chips (eg, K60Fxxxx12/15 etc) use the later registers.

(AN4445  Rev. 1, 8/2012) Kinetis 100 MHz Rev 1.x to Rev 2.x Migration Guide

It describes all of the differences I have found and many more besides.  So at least I'm not going mad......... !

Unfortunately, not realising these differences, our off-site hardware developer has used Issue 1 chips on his prototype PCBs, whereas we will use Issue 2s on our Production boards.  So I have to support both varieties for now.

So I suggest Freescale updates its examples to use the later registers etc so future developers don't get caught by this.


View solution in original post

0 Kudos
Reply
1 Reply
1,873 Views
neillewis
Contributor II

I did more research and happened upon this document describing the differences between Issue 1 and Issue 2 of the K60 100 MHz chips.  As far as I can tell the later 120 and 150 MHz chips (eg, K60Fxxxx12/15 etc) use the later registers.

(AN4445  Rev. 1, 8/2012) Kinetis 100 MHz Rev 1.x to Rev 2.x Migration Guide

It describes all of the differences I have found and many more besides.  So at least I'm not going mad......... !

Unfortunately, not realising these differences, our off-site hardware developer has used Issue 1 chips on his prototype PCBs, whereas we will use Issue 2s on our Production boards.  So I have to support both varieties for now.

So I suggest Freescale updates its examples to use the later registers etc so future developers don't get caught by this.


0 Kudos
Reply