MK60DN512VLL10R MCU USB power pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60DN512VLL10R MCU USB power pins

3,329 Views
markheiberger
Contributor I

We intend to use NXP’s MK60DN512VLL10R MCU in a new product. Can we leave pins 12 (VOUT33) & 13 (VREGIN) disconnected(floating). We do not intend to use USB power. Also, the datasheet states that pin 12 should/must have a capacitor attached. But, it can’t be more than 8.16uF. We are shipping product with 10uF on this pin. What kind of problems could this cause?

0 Kudos
Reply
3 Replies

3,222 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Mark,

If you don't  use USB, both VOUT33 and VREGIN should tie to output and ground through 10k resistor. If you still need USB but not use VOUT33, you can refer to https://community.nxp.com/message/965047?commentID=965047#comment-965047 

If you don't use USB, VOUT33 connect with a 10uF cap will not cause any problem.

But if you still use USB, the above link will give you some answer too.

Regards,

Jing

0 Kudos
Reply

3,220 Views
markheiberger
Contributor I

Hi Jing,

So this note from the product literature is no longer correct?

Thanks,

Mark

0 Kudos
Reply

3,220 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, this is noted on the reference manual. Then floating those pins please. May other kinetis device datasheet says tie to ground via 10k resistor, like k22 and k64.

Regards,

Jing

0 Kudos
Reply