MK60DN512VLL10R MCU USB power pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK60DN512VLL10R MCU USB power pins

2,205 次查看
markheiberger
Contributor I

We intend to use NXP’s MK60DN512VLL10R MCU in a new product. Can we leave pins 12 (VOUT33) & 13 (VREGIN) disconnected(floating). We do not intend to use USB power. Also, the datasheet states that pin 12 should/must have a capacitor attached. But, it can’t be more than 8.16uF. We are shipping product with 10uF on this pin. What kind of problems could this cause?

0 项奖励
回复
3 回复数

2,098 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Mark,

If you don't  use USB, both VOUT33 and VREGIN should tie to output and ground through 10k resistor. If you still need USB but not use VOUT33, you can refer to https://community.nxp.com/message/965047?commentID=965047#comment-965047 

If you don't use USB, VOUT33 connect with a 10uF cap will not cause any problem.

But if you still use USB, the above link will give you some answer too.

Regards,

Jing

0 项奖励
回复

2,096 次查看
markheiberger
Contributor I

Hi Jing,

So this note from the product literature is no longer correct?

Thanks,

Mark

0 项奖励
回复

2,096 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, this is noted on the reference manual. Then floating those pins please. May other kinetis device datasheet says tie to ground via 10k resistor, like k22 and k64.

Regards,

Jing

0 项奖励
回复