MK60DN256 CPUID 0x410FC24 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK60DN256 CPUID 0x410FC24 ?

ソリューションへジャンプ
1,906件の閲覧回数
nico547845
Contributor I

Hello

I Have been using MK60DN256VLL for years and the CPUID during programming has always been 0x410FC241.

We have some chips from a different source and the CPUID is now 0x410FC240. Our code doesn't seem to run, how can I decode this CPUID to understand what is going on ?

 

Thanks

0 件の賞賛
返信
1 解決策
1,900件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nico547845,

CPUID Base Register
[3:0] Revision Revision number, the p value in the rnpn product revision identifier:
0x0 = Patch 0
0x1 = Patch 1

Patch 0.pngPatch 1.png

Would you please show the photo of these two MCUs? Check the part number(first line) and mask set(second line), there may some different between these two MCUs.
This is the photo of MCU on TWR-K60N512 during debug I can see the CPUID=0x410FC240

MCU photo.jpg

SCB_CPUID 0x410fc240.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,859件の閲覧回数
nico547845
Contributor I

Thank you for your help Robin, all clear now.

0 件の賞賛
返信
1,886件の閲覧回数
nico547845
Contributor I

Hi Robin 

The chips I have problems with are 

MK60DN256ZVLL10

4N30D

The ones that work 

MK60DN256VLL10

5N22D

 

 

0 件の賞賛
返信
1,869件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

AN4445 Kinetis 100 MHz Rev 1.x to Rev 2.x Migration Guide will show you the difference between MK60DN256VLL10 and MK60DN256ZVLL10. The program developed for MK60DN256VLL10 cannot be run directly on MK60DN256ZVLL10 without modification.

0 件の賞賛
返信
1,901件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nico547845,

CPUID Base Register
[3:0] Revision Revision number, the p value in the rnpn product revision identifier:
0x0 = Patch 0
0x1 = Patch 1

Patch 0.pngPatch 1.png

Would you please show the photo of these two MCUs? Check the part number(first line) and mask set(second line), there may some different between these two MCUs.
This is the photo of MCU on TWR-K60N512 during debug I can see the CPUID=0x410FC240

MCU photo.jpg

SCB_CPUID 0x410fc240.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信