MK30VLL7 5V-LCD drive problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK30VLL7 5V-LCD drive problem

ソリューションへジャンプ
1,831件の閲覧回数
blurblur
Contributor II

Hi. I am using K30VLL7 to drive my 5V LCD. The problem is when I want to setup from the processor expert, it didnt allow me to set 5V LCD. It says " 5V LCD not supported by HW". What does it mean?? But from the datasheet, as I understand,this micon is able to drive 5V LCD. Is there any other setting that I should change?

I use CPSEL=1, VSUPPLY=1, RVEN=1. Any other setting that I should set?

Can someone help. TQ

ラベル(1)
0 件の賞賛
返信
1 解決策
1,729件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi norzilash,

      The PE component SegLCD_LDD really have the 5V selection problem, I think it is the PE bug, I will report it to the Processor Expert development team. They will fix it.

    Now, you can use the code which is controlled by the register, about the configuration, I have a CW10.6 project for K40D100, you can refer to it.

Wish it helps you!

If you still have question, please contact with me!
Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,730件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi norzilash,

      The PE component SegLCD_LDD really have the 5V selection problem, I think it is the PE bug, I will report it to the Processor Expert development team. They will fix it.

    Now, you can use the code which is controlled by the register, about the configuration, I have a CW10.6 project for K40D100, you can refer to it.

Wish it helps you!

If you still have question, please contact with me!
Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,729件の閲覧回数
blurblur
Contributor II

Hi Jingjing,

Thanks for the reply and project reference file. TQ. Hope it will help. Thanks a lot.

Thank you,

illa

0 件の賞賛
返信
1,729件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi  illa,

    You are welcome!

    If you still have question, you can let me know!

    If this post is answered, please mark the correct answer button, thank you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信