MK28F JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK28F JTAG

1,661件の閲覧回数
andrew58210
Contributor II

We are using MK28FN2M0AVMI15 and are having issues connecting to a custom board with the Saegger J-link.  I noticed in the datasheet it talks about a "JTAG limited voltage range electricals" and "JTAG full voltage range electricals".  We are using 1.8V cpu supply and 1.2V core.  I noticed the "JTAG limited voltage range electricals" does not allow 1.8V.  So what does limited voltage mean?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,610件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Andrew,

 

This means the measurements were made through a limited range in voltage, from 2.7 to 3.6V. On the other hand, the measurements of the full range were taken from 1.71 to 3.6.

 

Regarding your setup, as you are using 1.8V then you should get results near the full range voltage electricals.

 

Hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信