MK22FN512VLL12 wafer changes and performance differences

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK22FN512VLL12 wafer changes and performance differences

5,208件の閲覧回数
jiangzz
Contributor II

The new batch of materials cannot accept the boot loader. Their silk screen marking is XE (batch 2019). I took the parts we could accept the boot loader normally (silk screen marking is PK, batch 2021) to compare. X-ray is as the attachment.

Please help me confirm whether they have changed the wafer. If so, what has changed between them? Is the ID the same?

[6FZ2F_MO}62}TL`]_WX(M2.png

picture 1

XIJ`)RAPQQVH2OSAIHKBR`G.png

picture 2 

F]$3A$JVT@@8_ZB[4X(]_}Y.png

 picture 3

_DNG$@)9VBY2T)949(R%(49.png

 picture 4

 

O_`%2}C76T[%%IDWKQ~19FX.png

 

picture 5

0 件の賞賛
返信
8 返答(返信)

5,192件の閲覧回数
ErichStyger
Specialist I

Because to me you have a different PCB, I would first check that part. Other than that, I have a list of check points here: https://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/

I hope this helps,

Erich

0 件の賞賛
返信

5,176件の閲覧回数
jiangzz
Contributor II

Our problem is that we can't accept the boot loader

XD3)S9`51WG6W}V18J_}WW4.png

 

`]K$})51K73H2@DV]W2G_[Q.png

 

The last picture in the second picture is as follows:

K61DK_R%{}{W2IRQJZ0NUXI.png

 As you can see, when accept the boot loader for the faulty chip (the silk screen is AE), his RST is faulty.

  The one in the upper left corner of the figure below.

[KK]E{X)K7T@OVNV6MAYN9U.png

 

We mainly want to know whether the firmware burned by these two different silk screen printed chips is consistent when they leave the factory, and whether the hardware design around them is consistent. Otherwise, according to our understanding, they will not be unable accept the boot loader.

0 件の賞賛
返信

5,158件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry maybe you have a counterfeit part

 

Where did you buy your part?

 

Regards

 

0 件の賞賛
返信

5,133件の閲覧回数
jiangzz
Contributor II

This reply is missing, but he said that the Xe is an engineering sample version. He didn't look at my problem carefully. We cannot accept the boot loader. Its silk screen is AE (xnae1935u). The silk screen of the chip that can accept the boot loader is PK (xnpk2144u). This chip was launched in 2014. Its chip shows that it has a date code, 1935 means 35 weeks in 2019. It will be a mass production version by 2019, Where is the theory of engineering first run samples version?@bobpaddock .

333.png

 

0 件の賞賛
返信

5,125件の閲覧回数
bobpaddock
Senior Contributor III

Which is why I deleted my reply when I realized my error.
It is part numbers that start with X or have a prefix of X.
Not part numbers that have X in some other place.

5,127件の閲覧回数
troelsoesteraa
Contributor III

Hi,
I think Bob is incorrect.
NXP doesn't actually want to disclose much of what the last line means, but luckily Mouser still stores an old PCN with some information:

https://www.mouser.com/PCN/Freescale_16780.pdf

Items starting with Q are assembled and tested at site in Kuala Lumpur, Malaysia
Items starting with XN are assembled and tested at Fujitsu-Nantong, China.
Wafer identifiers/lot code is AE or PK.

The first prototype Kinetis processors where pre-fixed by P instead of M. That's why some of the first prototypes were called e.g. PK22FN512VLL12, but they're from 2013/14 and long since gone.

0 件の賞賛
返信

5,203件の閲覧回数
ErichStyger
Specialist I

The new batch of materials cannot accept the boot loader.

I'm not sure what you mean with this. What is the problem? Are you not able to debug it?

As for your pictures: they are interesting, mostly they show a different PCB underneath with different traces/vias. And you see the packaging pins/leads/traces, but not the silicon itself with details.

As for the marking /differences: have you already checked the errata/version/marking information if it is indeed a different silicon revision or just a a different packaging series?

Erich

0 件の賞賛
返信

5,199件の閲覧回数
jiangzz
Contributor II

Yes, we can't debug it.

0 件の賞賛
返信