MK22FN512 register layout typedefs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK22FN512 register layout typedefs

ソリューションへジャンプ
1,970件の閲覧回数
errorek123
Contributor III

Hi,

Recently i started digging more into files provided by NXP and i found out something i can't really explain. My question is how exactly uint8_t array of 252 elements gives 100 offset? Could u please clear that out? Thanks :smileyhappy:

zdj1.PNG

zdj2.PNG

0 件の賞賛
返信
1 解決策
1,885件の閲覧回数
mjbcswitzerland
Specialist V

Hi Brian

PIT_MCR is at address 0x40037000 and is 32 bits in size (and thus occupies 4 bytes)
Add 252 bytes to that and you get to the offset 256.

In the struct PIT_LDVAL will therefore be a 0x40037100 (0x40037000 + 4 + 252)

Regards

Mark


Complete Kinetis solutions, training and support: http://www.utasker.com/kinetis.html
Kinetis K22:
- http://www.utasker.com/kinetis/FRDM-K22F.html
- http://www.utasker.com/kinetis/TWR-K22F120M.html
- http://www.utasker.com/kinetis/BLAZE_K22.html
- http://www.utasker.com/kinetis/tinyK22.html

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,885件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Brian Smith,

   Mark's reply is correct, please refer to it.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,886件の閲覧回数
mjbcswitzerland
Specialist V

Hi Brian

PIT_MCR is at address 0x40037000 and is 32 bits in size (and thus occupies 4 bytes)
Add 252 bytes to that and you get to the offset 256.

In the struct PIT_LDVAL will therefore be a 0x40037100 (0x40037000 + 4 + 252)

Regards

Mark


Complete Kinetis solutions, training and support: http://www.utasker.com/kinetis.html
Kinetis K22:
- http://www.utasker.com/kinetis/FRDM-K22F.html
- http://www.utasker.com/kinetis/TWR-K22F120M.html
- http://www.utasker.com/kinetis/BLAZE_K22.html
- http://www.utasker.com/kinetis/tinyK22.html

0 件の賞賛
返信