MK22FN1M0V12 Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK22FN1M0V12 Question

2,252 Views
sudhanshumehta
Contributor IV

Is there in any option for using "MQX + Processor Expert + KDS" (without KSDK) on Kinetics MK22FN1M0V12.

if yes, do we have any work instructions or example project?

3 Replies

1,845 Views
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately the MQX 4.2 doesn't have bsp projects with PE enabled for the KDS, I suggest to use the PE standalone tool in order to generate code and copy the needed functions.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,845 Views
sudhanshumehta
Contributor IV

Hi Sol,

Thanks for the feedback. 

Do yo have any good document/help to start with...

Is this is something related to component  development environment

https://nxp.flexnetoperations.com/control/frse/download?element=5998621 

Thanks

Sudhanshu

0 Kudos
Reply

1,845 Views
soledad
NXP Employee
NXP Employee

You can check the below documents:

Creating a New MQX RTOS 4.2 project in KDS 

How to add RTCS to a Processor Expert Project Using KDS and KSDK 

How to add MFS and Shell support to a new MQX RTOS for KSDK and PEx project 

I hope this helps, have a nice day!

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply