MK20DX128VLF5 : differences between mask sets

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK20DX128VLF5 : differences between mask sets

2,021件の閲覧回数
Fendra22
Contributor I

Hi,

I own 2 different mask sets of MK20DX128VLF5 : 1N86B and 3N86B.

My system is working on the 3N86B. Should I expect problems when I switch to the 1N86B version?

How can I know the differences between the two mask sets?

Thank you for the help.

 

タグ(4)
0 件の賞賛
返信
1 返信

2,010件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Thank you so much again for using our community.

Each type or version of the MCU has its own mask which corresponds to the entire circuitry of the MCU. This mask set corresponds to the errata list which can be considered when MCU is used. Please refer to the following Mask Set Errata 1N86B and 3N86B to check the differences between them and if it is compatible with your application.

I hope this will help you. Please let me know if you have more questions about it.

0 件の賞賛
返信