MK20DX128VFM5 IAR EWARM Source Code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK20DX128VFM5 IAR EWARM Source Code

1,878 Views
fezaifethi
Contributor I

Hello, 

we want to use the MK20DX128VFM5  for our project , the probleme is I'm a little bit confused, I can't found the source code (library + example for this component)
I want to know, If I can use the TWR-K20D50M 's Firmware?
Or should we, change the chip?
Best regards,
Fezai

2 Replies

1,777 Views
miduo
NXP Employee
NXP Employee

Hi,

Yes, you can use TWR-K20D50M as an evaluation board. You can download the sample code for the board from the link below:

http://www.nxp.com/assets/downloads/data/en/board-support-packages/TWR-K20D50M_LABS_AND_CE.zip 

1,777 Views
fezaifethi
Contributor I

Hi Fang Li,

Thank you for your fast reply. 

0 Kudos
Reply