MK20DN512VLQ10 EZP_MS bit question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK20DN512VLQ10 EZP_MS bit question

921 次查看
isaotakashima
Contributor IV

I would like to migrate from MK20DN512ZVLQ10 to MK20DN512VLQ10.

I refer the  AN4445 Kinetis 100 MHz Rev 1.x to Rev 2.x Migration Guide, and I have the question.

The description of EZP_MS bit of Mode Register (RCM_MR) is as below, but I cannot find out the EZP_MS in the Chapter 10 Signal Multiplexing and Signal Descriptions.

EZP_MS_B pin state
Reflects the state of the EZP_MS pin during the last Chip Reset
0 Pin deasserted (logic 1)
1 Pin asserted (logic 0)

I believe that EZP_MS_B (EZP_MS) is wrong, EZP_CS_B (EZP_CS) should be correct.

Am I correct?

Please reply as soon as possible.

Best regards,

Takashima

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

821 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Takashima,
Yes you are right. The "EZP_MS pin" in the RCM_MR register should be "EZP_CS pin". It only change the register address, not the function.
Thank you very much.
Regards
Jing

0 项奖励
回复