MK20 SPI doesn't work with disabled FIFO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK20 SPI doesn't work with disabled FIFO

3,362 Views
marcusguenther
Contributor I

if I try to use the SPI0 of a MK20DX256 with disabled TX and RK FIFO it doesn't work.

I tried nearly everthing. I use the Config-Tool of Prozessor Expert (only the Init-Module) to set the Init-Parameter.

But regardless what I do I got only the frame below.

I init the device (see code below) and write 0xAA the TX_DATA in PUSHR. As you can see it is transmitted but the CS is only a peak

and after this transmission I can do what I want, nothing happens anymore :-( I got no more frames until doing a reset.

Have anyone an idea?

DS4_QuickPrint1.png

#define STOP_TRANSFER(x) (SPI0_MCR |= SPI_MCR_HALT_MASK);

#define START_TRANSFER (SPI0_MCR |= SPI_MCR_HALT_MASK);

#define SET_CONT_SCKE(x) (SPI0_MCR |= (((uint32)(x & 0x01) << SPI_MCR_CONT_SCKE_SHIFT) & SPI_MCR_CONT_SCKE_MASK))

//Clear the TX FIFO counter

#define CLR_RXF (SPI0_MCR |= SPI_MCR_CONT_SCKE_MASK) 

// Clear Transfer Counter

#define CLR_CTCNT (SPI0_PUSHR |= SPI_PUSHR_CTCNT_MASK)

#define SET_CS_CONT(x) (SPI0_PUSHR = SPI0_PUSHR |(((x & 0x01) << SPI_PUSHR_CONT_SHIFT) & SPI_PUSHR_CONT_MASK))

#define SET_PUSHR(command,data) (SPI0_PUSHR = (uint32)command + data)

#define SET_TX_DATA(data) (SPI0_PUSHR = (SPI0_PUSHR & 0xFFFF0000) + data)

#define GET_RX_DATA ((uint8)SPI0_RXFR0)

// Transfer complete? 0 Transfer not complete /  1 Transfer complete

#define GET_TCF ((uint8)((SPI0_SR & SPI_SR_TCF_MASK) >> SPI_SR_TCF_SHIFT))

#define CLR_TCF (SPI0_SR &= ~SPI_SR_TCF_MASK)

// Receive complete? 0 RX FIFO is empty / 1 RX FIFO is not empty

#define GET_RFDF ((uint8)((SPI0_SR & SPI_SR_RFDF_MASK) >> SPI_SR_RFDF_SHIFT))

// this function I call in main()

void Write_Test_Byte(void)

{

// SET_CS_CONT(1); //

// CLR_CTCNT;

// CLR_RXF;

  SPI0_PUSHR = (SPI0_PUSHR & 0xFFFF0000) + 0xAA; // send byte

  // }

// else return(TRANSMISSION_IS_RUNNING);

  for(uint32 j=0; j < 10000; j++)

  {

  NOP; // wait a while

  }

  // here breakpoint

// CLR_CTCNT;

// CLR_TCF;

}

/*

** ===================================================================

**     Method      :  SPI0_Init (component Init_SPI)

**     Description :

**         This method initializes registers of the SPI module

**         according to the Peripheral Initialization settings.

**         Call this method in user code to initialize the module. By

**         default, the method is called by PE automatically; see "Call

**         Init method" property of the component for more details.

**     Parameters  : None

**     Returns     : Nothing

** ===================================================================

*/

void SPI0_Init(void)

{

  /* SIM_SCGC6: SPI0=1 */

  SIM_SCGC6 |= SIM_SCGC6_SPI0_MASK;                                  

  /* SPI0_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=0,DOZE=0,MDIS=0,DIS_TXF=0,DIS_RXF=0,CLR_TXF=0,CLR_RXF=0,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */

  SPI0_MCR = SPI_MCR_DCONF(0x00) |

             SPI_MCR_PCSIS(0x00) |

             SPI_MCR_SMPL_PT(0x00) |

             SPI_MCR_HALT_MASK;      

  /* SPI0_MCR: MSTR=1,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=1,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=1,DOZE=0,MDIS=0,DIS_TXF=1,DIS_RXF=1,CLR_TXF=1,CLR_RXF=1,SMPL_PT=2,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */

  SPI0_MCR = SPI_MCR_MSTR_MASK |

             SPI_MCR_DCONF(0x00) |

             SPI_MCR_MTFE_MASK |

             SPI_MCR_PCSIS(0x01) |

             SPI_MCR_DIS_TXF_MASK |

             SPI_MCR_DIS_RXF_MASK |

             SPI_MCR_CLR_TXF_MASK |

             SPI_MCR_CLR_RXF_MASK |

             SPI_MCR_SMPL_PT(0x02) |

             SPI_MCR_HALT_MASK;      

  /* SPI0_TCR: SPI_TCNT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SPI0_TCR = SPI_TCR_SPI_TCNT(0x00);                                  

  /* SPI0_CTAR0: DBR=0,FMSZ=7,CPOL=1,CPHA=0,LSBFE=0,PCSSCK=3,PASC=3,PDT=3,PBR=1,CSSCK=5,ASC=5,DT=5,BR=7 */

  SPI0_CTAR0 = SPI_CTAR_FMSZ(0x07) |

               SPI_CTAR_CPOL_MASK |

               SPI_CTAR_PCSSCK(0x03) |

               SPI_CTAR_PASC(0x03) |

               SPI_CTAR_PDT(0x03) |

               SPI_CTAR_PBR(0x01) |

               SPI_CTAR_CSSCK(0x05) |

               SPI_CTAR_ASC(0x05) |

               SPI_CTAR_DT(0x05) |

               SPI_CTAR_BR(0x07);      

  /* SPI0_CTAR1: DBR=0,FMSZ=3,CPOL=1,CPHA=0,LSBFE=0,PCSSCK=0,PASC=0,PDT=0,PBR=0,CSSCK=0,ASC=0,DT=0,BR=0 */

  SPI0_CTAR1 = SPI_CTAR_FMSZ(0x03) |

               SPI_CTAR_CPOL_MASK |

               SPI_CTAR_PCSSCK(0x00) |

               SPI_CTAR_PASC(0x00) |

               SPI_CTAR_PDT(0x00) |

               SPI_CTAR_PBR(0x00) |

               SPI_CTAR_CSSCK(0x00) |

               SPI_CTAR_ASC(0x00) |

               SPI_CTAR_DT(0x00) |

               SPI_CTAR_BR(0x00);      

  /* SPI0_SR: TCF=1,TXRXS=0,??=0,EOQF=1,TFUF=1,??=0,TFFF=1,??=0,??=0,??=0,??=0,??=0,RFOF=1,??=0,RFDF=1,??=0,TXCTR=0,TXNXTPTR=0,RXCTR=0,POPNXTPTR=0 */

  SPI0_SR = SPI_SR_TCF_MASK |

            SPI_SR_EOQF_MASK |

            SPI_SR_TFUF_MASK |

            SPI_SR_TFFF_MASK |

            SPI_SR_RFOF_MASK |

            SPI_SR_RFDF_MASK |

            SPI_SR_TXCTR(0x00) |

            SPI_SR_TXNXTPTR(0x00) |

            SPI_SR_RXCTR(0x00) |

            SPI_SR_POPNXTPTR(0x00);      

  /* SPI0_RSER: TCF_RE=0,??=0,??=0,EOQF_RE=0,TFUF_RE=0,??=0,TFFF_RE=0,TFFF_DIRS=0,??=0,??=0,??=0,??=0,RFOF_RE=0,??=0,RFDF_RE=0,RFDF_DIRS=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SPI0_RSER = 0x00U;                                  

  /* SPI0_MCR: HALT=0 */

  SPI0_MCR &= (uint32_t)~(uint32_t)(SPI_MCR_HALT_MASK);                                  

}

Labels (1)
0 Kudos
Reply
4 Replies

2,795 Views
marcusguenther
Contributor I

yes, I got the same number of frames.... I resolved it in an another way meanwhile.... Thanks!

0 Kudos
Reply

2,795 Views
martynhunt
NXP Employee
NXP Employee

Hi Marcus,

Try this in your transmit function:

    SPI0_PUSHR |= (0x00010000 | 0xAA);


This should assert PCS0. If that doesn't work, let me know. Thank you.


Best regards,


Martyn

2,795 Views
marcusguenther
Contributor I

Yes this works... but leaded to the next problem.

After a reset and the Hardware Init-Routine of SPI0 the TCF is always 0. I have to send a dummy frame to clear it.

Futhermore I got with this code only to frames. If I have a breakpoint between the commands and execute it step by step

each command send a frame (3 frames). Without breakpoints I got only two frames. Isn't the device already ready when the TCF

is set? Never I had such probems with a SPI device :-(

#define GET_TCF(SPI0_SR & SPI_SR_TCF_MASK)

SPI0_PUSHR = 0x000100FF;
while(!GET_TCF);
SPI0_PUSHR = 0x000100FF;
while(!GET_TCF);
SPI0_PUSHR = 0x000100FF;
while(!GET_TCF);

NOP;

(no command is sent befor this code)

DS4_QuickPrint3.png

0 Kudos
Reply

2,795 Views
martynhunt
NXP Employee
NXP Employee

Hi Marcus,

Do you get the same number of frames if you remove the "while(!GET_TCF);" lines from your code? Also, are you still using your original register settings or have you changed them?

Thank you,

Martyn

0 Kudos
Reply