MK10FN1M0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK10FN1M0

1,903件の閲覧回数
XQ
Contributor I

大家好,我是新手,我目前正在开发MK10FN1M0的缓存驱动程序,但是我在官方网站上找不到相关信息。我在这里寻求您的帮助。可以给我一个相关的缓存案例以供参考吗?

0 件の賞賛
返信
3 返答(返信)

1,900件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

去官网下个sdk, 

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

有个Kinetis 120MHz bare metal sample code

或者去https://mcuxpresso.nxp.com/

里面sdk可能不是你的板子,但是两个mcu是同个结构,同样能用的。在sdk里翻翻你需要的内容吧

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,896件の閲覧回数
XQ
Contributor I

hi!,

    Hello, first of all thank you for helping me answer this question. I downloaded what you said. The function of the cache driver is not perfect, and the cache is not used in the example. It is simply defined in the driver layer. I want to know how to use this cache?

0 件の賞賛
返信

1,888件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

You can refer the k64's code.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信