MK10 series P-Flash question about Read/Write for bootload

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK10 series P-Flash question about Read/Write for bootload

Jump to solution
10,448 Views
eunseokjung
Contributor II

Hi all.

I have trouble to writing p-flash area for coding bootload.

Basically my code is depending on AN2295 SW.

I want to write some word like 0x2143. But it is not writing at the address 0x0410. It is written at 0x1FFF8000. Here is SRAM area.

My modified code is blow:

__attribute__((section(".programbuff"))) Byte buffer[200];

FCC0B_STR CommandObj;

#define FLASH_FlashCommandSequence ((LWord (*)(Byte))&buffer[1])

FLASH_ProgramLongWord(destination, *pSource++)

{

    CommandObj.regsLong.fccob3210 = destination;

    CommandObj.regs.fccob0 = FLASH_PROGRAM_LONGWORD;

    CommandObj.regsLong.fccob7654 = data32b;

  return FLASH_FlashCommandSequence(PROGRAM_LONGWORD_INDEX);

}

I set the destination 0x410

*pSource is data array pointer.

But it write at 0x1FFF8000 not 0x0410.

Error message is this: No source available for "0x1FFF8000 (0x1FFF8000)() "

What is meaning of #define FLASH_FlashCommandSequence((LWord (*)(Byte))&buffer[1]) ?

Why i need this? and What is FCC0B STR CommandObj? I can't understand this meaning.

And my syntax is right?

Do you have idea?

Thank you.

Eunseok.

Labels (1)
0 Kudos
Reply
1 Solution
9,943 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eunseok Jung,

      FLASH_FlashCommandSequenceStart function is used for the flash command operation sequence.

    As you know, every flash operation is using the according command to realize the flash operation function by write the FCCOBx register.

    The index is means how many FCCOB register to control, the base address is defined as FLASH_BASE_PTR->FCCOB3:Just FCCOB3,

  From our flash register table, you will know FCCOB3 is the base address of FCCOBn, just like the following:

pastedImage_1.png

#define ERASE_BLOCK_INDEX      4

#define PROGRAM_LONGWORD_INDEX  8

#define PROGRAM_PHRASE_INDEX    12

The index number should be the number of FCCOB registers which need to control.

(1)ERASE_BLOCK_INDEX 4  means Erase block is just control 4 FCCOB registers:

pastedImage_0.png

(2) PROGRAM_LONGWORD_INDEX 8 means  this command should control 8 FCCOB registers:

pastedImage_3.png

(3) PORGRAM_PHASE_INDEX 12

I think it should be the Progarm check command, this command should control 12 FCCOB registers:

pastedImage_0.png

Please find more detals from our K10 reference manual, chapter 29 .

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
14 Replies
9,943 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eunseok Jung,

    Alice Yang is correct.

    In your code, you do the following definition:

   for(i = 0;i<10; i++)
     {
write_buffer[i] = 0x2143;
       //#if BOOTLOADER_CRC_ENABLE == 1
       //  CRC_AddByte(write_buffer[i]);
       //#endif
     }

That's why you see your 0x2143 in the RAM address, because you define it in the RAM.

Before you do flash writing , you should erase it at first, otherwise , your flash operation won't be successed.

Actually, in AN2295, from address 0x00000410, it is the bootloader code.

pastedImage_1.png

I don't know, why you write the word 0x2143 in the bootloader code area.

If you want to realize the function of uart bootloader, you need to modify your application code address, not the bootloader code address.

Please read our AN2295.pdf at first, this application write how to realize the uart bootloader in details, please read Chapter 7 carefully.

If you stll have quesiton, please let us know.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
9,943 Views
eunseokjung
Contributor II

Thank you Jingjing.

The reason why i want to write at 0x0000410 is just practice for bootload.

Can i ask one?

Could you explain this function? It is from AN2295SW file.

LWord FLASH_FlashCommandSequenceStart(Byte index)

{

  Byte* ptrFccobReg = (Byte*)&FLASH_BASE_PTR->FCCOB3;

  Byte* ptrCommandObj = (Byte*)&CommandObj;

  /* wait till CCIF bit is set */

  while(!(FLASH_FSTAT & FLASH_FSTAT_CCIF_MASK)){};

  /* clear RDCOLERR & ACCERR & FPVIOL flag in flash status register */

  FLASH_FSTAT = FLASH_FSTAT_ACCERR_MASK | FLASH_FSTAT_FPVIOL_MASK | FLASH_FSTAT_RDCOLERR_MASK;

  /* load FCCOB registers */

  while(index--)

    *ptrFccobReg++ = *ptrCommandObj++;

  //  launch a command

  FLASH_FSTAT |= FLASH_FSTAT_CCIF_MASK;

  //  waiting for the finishing of the command

  while(!(FLASH_FSTAT & FLASH_FSTAT_CCIF_MASK)){};

   /* Check error bits */

  /* Get flash status register value */

  return (FLASH_FSTAT & (FLASH_FSTAT_ACCERR_MASK | FLASH_FSTAT_FPVIOL_MASK | FLASH_FSTAT_MGSTAT0_MASK));

}

One more question.

In AN2295SW file, they defined some indexes.

#define ERASE_BLOCK_INDEX       4

#define PROGRAM_LONGWORD_INDEX  8

#define PROGRAM_PHRASE_INDEX    12

Why ERASE BLOCK INDEX is 4 and why LONGWORD is 8 and phrase is 12?

Could you help me?

BR

Eunseok.

0 Kudos
Reply
9,944 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eunseok Jung,

      FLASH_FlashCommandSequenceStart function is used for the flash command operation sequence.

    As you know, every flash operation is using the according command to realize the flash operation function by write the FCCOBx register.

    The index is means how many FCCOB register to control, the base address is defined as FLASH_BASE_PTR->FCCOB3:Just FCCOB3,

  From our flash register table, you will know FCCOB3 is the base address of FCCOBn, just like the following:

pastedImage_1.png

#define ERASE_BLOCK_INDEX      4

#define PROGRAM_LONGWORD_INDEX  8

#define PROGRAM_PHRASE_INDEX    12

The index number should be the number of FCCOB registers which need to control.

(1)ERASE_BLOCK_INDEX 4  means Erase block is just control 4 FCCOB registers:

pastedImage_0.png

(2) PROGRAM_LONGWORD_INDEX 8 means  this command should control 8 FCCOB registers:

pastedImage_3.png

(3) PORGRAM_PHASE_INDEX 12

I think it should be the Progarm check command, this command should control 12 FCCOB registers:

pastedImage_0.png

Please find more detals from our K10 reference manual, chapter 29 .

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
9,943 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Jung,

Please check the linker file ,the section".programbuff" is in which segment .

BR

Alice

0 Kudos
Reply
9,943 Views
eunseokjung
Contributor II

Programbuff is in

m_programbuff (RW) : ORIGIN = 0x1FFF8000, LENGTH = 0x00001000

Is this the reason for writing in 0x1FFF8000?

I changed the region

m_programbuff (RW) : ORIGIN = 0x020000, LENGTH = 0x00001000.

But it is not working properly.

The debug always error when it run #define FLASH_FlashCommandSequence ((LWord (*)(Byte))&buffer[1]) command.

And what is m_text segment(or session?) What is written  in here?

0 Kudos
Reply
9,943 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

HIi,

Which IDE do you use ?

Mainly fcous on the "SECTION " part of Linker file .

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

0 Kudos
Reply
9,943 Views
eunseokjung
Contributor II

I'm using CW10.3 with Multilink Universal.

I haven't SECTION part in the Linker file.

MEMORY {

  m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x000001BC

  m_text      (RX) : ORIGIN = 0x00000410, LENGTH = 0x0001FBF0

  m_data      (RW) : ORIGIN = 0x1FFF9000, LENGTH = 0x00007000

  m_data_20000000 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00008000

  m_programbuff (RW) : ORIGIN = 0x00020000, LENGTH = 0x00001000

  m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010

}

My code has problem when it runs "The debug always error when it run #define FLASH_FlashCommandSequence ((LWord (*)(Byte))&buffer[1])" command.

0 Kudos
Reply
9,943 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Could you send your project to me ?

0 Kudos
Reply
9,943 Views
eunseokjung
Contributor II

I uploaded my project file

0 Kudos
Reply
9,943 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

This is this the SECTION :

pastedImage_0.png

from this part , you can find the place of your  ".programbuff"  :

m_programbuff (RW) : ORIGIN = 0x00020000, LENGTH = 0x00001000

.........

  .m_programbuff : AT(___m_programbuff_ROMStart)

  {

     . = ALIGN(4);

     ___m_programbuff_RAMStart = .;

     *(.m_programbuff) /* This is an User defined section */

     ___m_programbuff_RAMEnd = .;

     . = ALIGN(4);

  } > m_programbuff

0 Kudos
Reply
9,943 Views
eunseokjung
Contributor II

I paste your code

.m_programbuff : AT(___m_programbuff_ROMStart)

  {

     . = ALIGN(4);

     ___m_programbuff_RAMStart = .;

     *(.m_programbuff) /* This is an User defined section */

     ___m_programbuff_RAMEnd = .;

     . = ALIGN(4);

  } > m_programbuff

in the section.

But the result is same. Error is same. It is not working....

0 Kudos
Reply
9,943 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Sorry you misunderstand me .

I just tell you how to check the Linker file,  to find the  setion ".programbuff" in it.

Now , i just find there is a error :

change this

   __attribute__((section(".programbuff"))) Byte buffer[200];

to

   __attribute__((section(".m_programbuff"))) Byte buffer[200];

.

And if still have question , please tell me what'e the problem , and what's your aim.

BR

Alice

0 Kudos
Reply
9,943 Views
eunseokjung
Contributor II

My problem is occurred when i run "#define FLASH_FlashCommandSequence ((LWord (*)(Byte))&buffer[0])" . It makes error.


I want write some value at 0x00020000.

But this code can't write at 0x00020000.This code write value at 0x1FFF9040 instead of 0x00020000.

How can i write value at 0x00020000.

Thank you~

0 Kudos
Reply
9,943 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

I think the 0x1fff9040 is the address of your write_buffer[i] , please check.

And it seems that you have not erase the flash you want to write.

And if your aim is simple write data to flash , you can not use the bootlaoder , can simple configurate the linker file.

BR

Alice

0 Kudos
Reply