MK10 PLL clock configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK10 PLL clock configuration

1,454 Views
davithakobyan
Contributor III

Hi,

I try to run a sample project for MK10DN512VLL10 by configuring the clock to use the external OSC and run at 100 MHz of PLL. However, the execution hangs in a while loop for waiting the clock source to be set to external clock reference. The relevant parts are as follows:

Configuration part

 

const mcg_config_t mcgConfig_BOARD_BootClockRUN =
    {
        .mcgMode = kMCG_ModePEE,                  /* PEE - PLL Engaged External */
        .irclkEnableMode = MCG_IRCLK_DISABLE,     /* MCGIRCLK disabled */
        .ircs = kMCG_IrcSlow,                     /* Slow internal reference clock selected */
        .fcrdiv = 0x1U,                           /* Fast IRC divider: divided by 2 */
        .frdiv = 0x0U,                            /* FLL reference clock divider: divided by 1 */
        .drs = kMCG_DrsLow,                       /* Low frequency range */
        .dmx32 = kMCG_Dmx32Default,               /* DCO has a default range of 25% */
        .oscsel = kMCG_OscselOsc,                 /* Selects System Oscillator (OSCCLK) */
        .pll0Config =
            {
                .enableMode = kMCG_PllEnableIndependent,/* MCGPLLCLK enabled independent of MCG clock mode, MCGPLLCLK disabled in STOP mode */
                .prdiv = 0x3U,                    /* PLL Reference divider: divided by 4 */
                .vdiv = 0x1aU,                    /* VCO divider: multiplied by 50 */
            },
    };
const sim_clock_config_t simConfig_BOARD_BootClockRUN =
    {
        .pllFllSel = SIM_PLLFLLSEL_MCGFLLCLK_CLK, /* PLLFLL select: MCGFLLCLK clock */
        .er32ksrc=SIM_OSC32KSEL_OSC32KCLK_CLK,  /* OSC32KSEL select: OSC32KCLK clock */
        .clkdiv1 = 0x1130000U,                    /* SIM_CLKDIV1 - OUTDIV1: /1, OUTDIV2: /2, OUTDIV3: /2, OUTDIV4: /4 */
    };
const osc_config_t oscConfig_BOARD_BootClockRUN =
    {
        .freq = 8000000U,                         /* Oscillator frequency: 8000000Hz */
        .capLoad = (OSC_CAP0P),                   /* Oscillator capacity load: 0pF */
        .workMode = kOSC_ModeExt,                 /* Use external clock */
        .oscerConfig =
            {
                .enableMode = OSC_ER_CLK_DISABLE, /* Disable external reference clock */
            }
    };

 

Setting up the clock

 

void BOARD_BootClockRUN(void)
{
    /* Set the system clock dividers in SIM to safe value. */
    CLOCK_SetSimSafeDivs();
    /* Initializes OSC0 according to board configuration. */
    CLOCK_InitOsc0(&oscConfig_BOARD_BootClockRUN);
    CLOCK_SetXtal0Freq(oscConfig_BOARD_BootClockRUN.freq);
    /* Configure FLL external reference divider (FRDIV). */
    CLOCK_CONFIG_SetFllExtRefDiv(mcgConfig_BOARD_BootClockRUN.frdiv);
    /* Set MCG to PEE mode. */
    CLOCK_BootToPeeMode(mcgConfig_BOARD_BootClockRUN.oscsel,
                        kMCG_PllClkSelPll0,
                        &mcgConfig_BOARD_BootClockRUN.pll0Config);
    /* Set the clock configuration in SIM module. */
    CLOCK_SetSimConfig(&simConfig_BOARD_BootClockRUN);
    /* Set SystemCoreClock variable. */
    SystemCoreClock = BOARD_BOOTCLOCKRUN_CORE_CLOCK;
}

 

The problem occurs in the above CLOCK_BootToPeeMode function. Particularly, it hangs in the following check:

 

    while ((MCG->S & (MCG_S_IREFST_MASK | MCG_S_CLKST_MASK)) !=
           (MCG_S_IREFST(kMCG_FllSrcExternal) | MCG_S_CLKST(kMCG_ClkOutStatExt)))
    {
    }

 

 

Does anyone know the reason why it is not possible to set the external ref. clock?

Does anyone have a working clock initialization procedure which one could use?

Thanks a lot in advance.

0 Kudos
Reply
1 Reply

1,442 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi davithakobyan,

Are you using an external crystal or external reference clock source?

Crystal or external reference clock.pngCrystal or external reference clock.png

Here is the difference:

clock tools.pngclock tools.png

In addition, you can also check if there is a matching errata.

Please check the mask of MCU, make sure the part number is MK10DN512VLL10 not MK10DN512ZVLL10

The codes shown below belong to CLOCK_BootToBlpeMode and CLOCK_SetPbeMode. Did you call these function?

    while ((MCG->S & (MCG_S_IREFST_MASK | MCG_S_CLKST_MASK)) !=
           (MCG_S_IREFST(kMCG_FllSrcExternal) | MCG_S_CLKST(kMCG_ClkOutStatExt)))
    {
    }

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply