MK10 Crystal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK10 Crystal

1,633 Views
aviamitai
Contributor I

Hi

We are using the MK10DX256 in one of our designs.

I am looking for the xtal drive level ,ESR ,load capacitance specification .

also is there a xtal preferred part list for the K10 family ? 

Regards,

Avi

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,488 Views
john_suchyta
NXP Employee
NXP Employee

Hi Avi,

We generally do not recommend crystals since there are so many vendors, and our chips can handle a wide range of frequencies. The MK10 crystal oscillator (EXTAL0/XTAL0) can operate in 2 modes - high gain and low power - and in 2 main frequency ranges - 32.768kHz and 3-30MHz. For the low frequency crystal, we recommend max ESR of 75k ohms and typical CL of 12.5pF. For a high frequency crystal we recommend max ESRs of 50 ohms for very high frequencies (32MHz) to 80 ohms for lower (8MHz) frequencies. Typical CL values are 18 to 20pF.

Smaller crystal packages tend to have higher ESR and lower CL, and should be used with caution. These can have longer startup times and may be difficult to tune with external load caps.

Regards,

John Suchyta

0 Kudos
Reply