MK10 (72MHz) External clock selection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MK10 (72MHz) External clock selection

跳至解决方案
1,787 次查看
donikuy
Contributor III

We need to select an external clock for a MK10 (72MHz).

What are the advantages/disatvantages of different external clock speeds when generating the internal speed.

We are trying to achieve 72MHz.

0 项奖励
回复
1 解答
1,621 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ylber Doniku,

      Thank you for your interest in Freescale kinetis product, I would like to provide service for you!

      If you want to use the crystal oscillator,  you can choose 3 to 32Mhz external crystal oscillator, this should use the internal OSC logic module, this module will have the power consumption, but to the external circuit, it is simple and low cost.

      If you want to use the external reference clock, the max input clock frequency is 50Mhz, and you should choose the proper frequency which can get 72Mhz.

the input clock duty cycle should in 40% to 60%.  This method don't need use the internal OSC logic module, so it can save the OSC consumption, but you need to use other clock generator component give the correct frequency.

    Actually, if you want to achieve 72Mhz, just refer to the TWR-K20D72M schematic, choose the external 8Mhz crystal is ok:

http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K20D72M_SCH1.pdf

Wish it helps you!

If you still have question, please contact me!
Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,622 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ylber Doniku,

      Thank you for your interest in Freescale kinetis product, I would like to provide service for you!

      If you want to use the crystal oscillator,  you can choose 3 to 32Mhz external crystal oscillator, this should use the internal OSC logic module, this module will have the power consumption, but to the external circuit, it is simple and low cost.

      If you want to use the external reference clock, the max input clock frequency is 50Mhz, and you should choose the proper frequency which can get 72Mhz.

the input clock duty cycle should in 40% to 60%.  This method don't need use the internal OSC logic module, so it can save the OSC consumption, but you need to use other clock generator component give the correct frequency.

    Actually, if you want to achieve 72Mhz, just refer to the TWR-K20D72M schematic, choose the external 8Mhz crystal is ok:

http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K20D72M_SCH1.pdf

Wish it helps you!

If you still have question, please contact me!
Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复