MK10 (72MHz) External clock selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK10 (72MHz) External clock selection

ソリューションへジャンプ
1,768件の閲覧回数
donikuy
Contributor III

We need to select an external clock for a MK10 (72MHz).

What are the advantages/disatvantages of different external clock speeds when generating the internal speed.

We are trying to achieve 72MHz.

0 件の賞賛
返信
1 解決策
1,602件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ylber Doniku,

      Thank you for your interest in Freescale kinetis product, I would like to provide service for you!

      If you want to use the crystal oscillator,  you can choose 3 to 32Mhz external crystal oscillator, this should use the internal OSC logic module, this module will have the power consumption, but to the external circuit, it is simple and low cost.

      If you want to use the external reference clock, the max input clock frequency is 50Mhz, and you should choose the proper frequency which can get 72Mhz.

the input clock duty cycle should in 40% to 60%.  This method don't need use the internal OSC logic module, so it can save the OSC consumption, but you need to use other clock generator component give the correct frequency.

    Actually, if you want to achieve 72Mhz, just refer to the TWR-K20D72M schematic, choose the external 8Mhz crystal is ok:

http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K20D72M_SCH1.pdf

Wish it helps you!

If you still have question, please contact me!
Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,603件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ylber Doniku,

      Thank you for your interest in Freescale kinetis product, I would like to provide service for you!

      If you want to use the crystal oscillator,  you can choose 3 to 32Mhz external crystal oscillator, this should use the internal OSC logic module, this module will have the power consumption, but to the external circuit, it is simple and low cost.

      If you want to use the external reference clock, the max input clock frequency is 50Mhz, and you should choose the proper frequency which can get 72Mhz.

the input clock duty cycle should in 40% to 60%.  This method don't need use the internal OSC logic module, so it can save the OSC consumption, but you need to use other clock generator component give the correct frequency.

    Actually, if you want to achieve 72Mhz, just refer to the TWR-K20D72M schematic, choose the external 8Mhz crystal is ok:

http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K20D72M_SCH1.pdf

Wish it helps you!

If you still have question, please contact me!
Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信