MK02FN64VLF10 UART Transfer Debug Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK02FN64VLF10 UART Transfer Debug Problem

2,463件の閲覧回数
jackxu2016
Contributor II

Hi there,

I want to using uart sends character to the pc as following

       /***************************************************************************

        * Defines

        **************************************************************************/  

         #define    DEMO_UART   UART1

         #define    BOARD_DEBUG_UART_BAUDRATE   115200

       /***************************************************************************

        * Variables

        **************************************************************************/  

         uint8_t   txbuff[] = "Uart polling example\r\nBoard will send back received characters\r\n";

         uint8_t   rxbuff[20] = {0};

       /***************************************************************************

        * Code

        **************************************************************************/  

         int main(void){

            uint8_t   ch;

            uart_config_t   config;

            

            /* Init board hardware*/

            BOARD_InitPins();

            BOARD_BootClockRUN();

            /*

             * config.baudRate_Bps = 115200U;

             * config.parityMode = kUART_ParityDisabled;

             * config.stopBitCount = kUART_OneStopBit;

             * config.txFifoWatermark = 0;

             * config.rxFifoWatermark = 1;

            */

            UART_Init(DEMO_UART, &config, CLOCK_GetFreq(kCLOCK_CoreSysClk));

            UART_WriteBlocking(DEMO_UART, txbuff, sizeof(txbuff) - 1);

            while(1)

           {

               UART_ReadBlocking(DEMO_UART, &ch, 1);

               UART_WriteBlocking(DEMO_UART, &ch, 1);

            }

         }

         void BOARD_InitPins(void){

            CLOCK_EnableClock(kCLOCK_PortA);

            CLOCK_EnableClock(kCLOCK_PortB);

            CLOCK_EnableClock(kCLOCK_PortC);

            CLOCK_EnableClock(kCLOCK_PortD);

            CLOCK_EnableClock(kCLOCK_PortE);

            PORT_SetPinMux(PORTC, 3U, kPORT_MuxAlt3);

            PORT_SetPinMux(PORTC, 4U, kPORT_MuxAlt3);

         }

kCLOCK_CoreSysClk      @40MHz

kCLOCK_BusClk               @40MHz

FEE   mode

         void UART_GetDefaultConfig(uart_config_t *config)

         {

            assert(config);

            config -> baudRate_Bps = 115200U;

            config -> parityMode = kUART_ParityDisabled;

         #if defined(FSL_FEATURE_UART_HAS_STOP_BIT_CONFIG_SUPPORT) && FSL_FEATURE_UART_HAS_STOP_BIT_CONFIG_SUPPORT

            config -> stopBitCount = kUART_OneStopBit;

         #endif

         #if defined(FSL_FEATURE_UART_HAS_FIFO) && FSL_FEATURE_UART_HAS_FIFO

            config -> txFifoWatermark = 0;

            config -> rxFifoWatermark = 1;

         #endif

            config -> enableTx = false;

            config -> enableRx = false;

         }

pastedImage_14.png

pastedImage_13.png

pastedImage_12.png

but when using FRDM-K22F runs uart_polling_transfer.c but SYSTEM_CLOCK @40MHz, BUS_CLOCK @40MHz, also in FEE mode, it runs good.

pastedImage_15.png

pastedImage_16.png

How can i fix the problem, the mk02 also can output the right message?

Thanks in advance!

-Jack

0 件の賞賛
返信
3 返答(返信)

2,162件の閲覧回数
jackxu2016
Contributor II

Hi Kerry,

Thanks for your quick answer, but i load two sample. one is base on frdm-k22f, and another is base on mk02fn64vlf10. when core system @40MHz, frdm-k22f can send the right message to the tera term with 115200bps, but the mk02fn64vlf10 can not send the right one with 115200bps.

Due to we set the clock at 40MHz, and as caculated  FRDM-K22F can send out the right message, but MK02FN64VLF10 can't

If MK02FN64VLF10 doesn't run at 40MHz, we also can not caculate the right one

UFRDM-K22F.jpg

MK02FN64VLF10.jpg

The 1st pic is from FRDM-K22F, the 2nd is from MK02FN64VLF10. both @115200bps

Need some more help, hope the 2nd one can send out right message!

Thanks in advance!

-Jack

0 件の賞賛
返信

2,162件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jack,

   You receive the messy code, it is normally caused by the baud rate skew.

   Normally, the baud rate deviation should smaller than 1.5%, otherwise the PC may receive the messy code.

  So, please debug the code, and check the UARTx_BDH and UARTx_BDL, then calculate the baud rate

UART baud rate = UART module clock / (16 × (SBR[12:0] + BRFD)),

 More details about the uart baud rate forum, please refer to chapter 40.4.3 Baud rate generation in the K02 reference manual.

 Please calculate your real baud rate, and compare with 115200, is the baud rate deviation larger than 1.5%?

 If yes, please reconfigure your UARTx_BDH and UARTx_BDL, to make sure the baud rate deviation should smaller than 1.5%.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,162件の閲覧回数
jackxu2016
Contributor II


/* Calculate the baud rate modulo divisor, sbr*/
sbr = srcClock_Hz / (baudRate_Bps * 16);

/* Write the sbr value to the BDH and BDL registers*/
base->BDH = (base->BDH & ~UART_BDH_SBR_MASK) | (uint8_t)(sbr >> 8);
base->BDL = (uint8_t)sbr;

#if defined(FSL_FEATURE_UART_HAS_BAUD_RATE_FINE_ADJUST_SUPPORT) && FSL_FEATURE_UART_HAS_BAUD_RATE_FINE_ADJUST_SUPPORT
/* Determine if a fractional divider is needed to fine tune closer to the
* desired baud, each value of brfa is in 1/32 increments,
* hence the multiply-by-32. */
uint16_t brfa = (32 * srcClock_Hz / (baudRate_Bps * 16)) - 32 * sbr;

/* Write the brfa value to the register*/
base->C4 = (base->C4 & ~UART_C4_BRFA_MASK) | (brfa & UART_C4_BRFA_MASK);
#endif

0 件の賞賛
返信