MK02 Not listed in processor choice KDS3.0.0 SDK1.2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK02 Not listed in processor choice KDS3.0.0 SDK1.2.0

1,460 Views
johnsteggall
Contributor I

Why can I not find the MK02 processor in the list? Is there another thing I have to do?

There was another thread on this for KDS2.0 but I cannot see the solution that is linked.

Thanks.

John.

Labels (1)
0 Kudos
Reply
5 Replies

1,294 Views
dave408
Senior Contributor II

Strange.  I'm running KDS 3.0 now and this is what I see:

pastedImage_0.png

0 Kudos
Reply

1,294 Views
diegocolombo
Contributor IV

Hi

I have it too,but it is not supported for debugging

Can you help me?

Thanks

0 Kudos
Reply

1,294 Views
dave408
Senior Contributor II

Hi Diego, I'm not familiar enough with that processor and KDS to know whether or not it would be supported for debugging.  I kind of assumed anything on the list was supported.  Can you be specific about what kind of problems you're having when you try to debug?  Posting error messages and screenshots would be helpful.

0 Kudos
Reply

1,294 Views
diegocolombo
Contributor IV

I was very very newbie in KDS.

I had to update with a more recent SDK and then add EMbSysRegView as explained in

How to Add Register Details View in Eclipse | MCU on Eclipse

Thanks to you all for the good hints

Diego

0 Kudos
Reply

1,294 Views
johnsteggall
Contributor I

Just read the instructions for the SDK. It's all there!

Ooops.

0 Kudos
Reply