MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,957件の閲覧回数
a8Chcx
Contributor V

Hi,

I have installed MCUXpresso IDE version 11.2.0 with FRDM-K66 SDK 2.8.0. Everything is working fine...

Today, I installed MCUXpresso IDE version 11.5.0 with FRDM-K66 SDK 11.0. It works fine...

When I close both IDEs and re-launch version 11.2.0 and it tells me that it can't find SDK2.8.0...

I have to re-install SDK 2.8.0 to make it work...

How can I set to use the specified SDK for the different IDE version as follows?

MCUXpresso IDE version 11.2.0 with FRDM-K66 SDK 2.8.0

MCUXpresso IDE version 11.5.0 with FRDM-K66 SDK 11.0

 

Thanks,

Christie

 

0 件の賞賛
返信
1 解決策
1,929件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @a8Chcx ,

It seems you let the two MCUXpresso share a SDK folder. You can assign different SDK folder to each IDE. It is in window->preferences

jingpan_0-1646968934381.png

 

Regards,

Jing

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,930件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @a8Chcx ,

It seems you let the two MCUXpresso share a SDK folder. You can assign different SDK folder to each IDE. It is in window->preferences

jingpan_0-1646968934381.png

 

Regards,

Jing

 

 

0 件の賞賛
返信