MCUExpresso IDE LinkServer (CMSIS DAP) probe sends a NULL to target ~87uSec after power up.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUExpresso IDE LinkServer (CMSIS DAP) probe sends a NULL to target ~87uSec after power up.

3,625件の閲覧回数
madisonchou
Contributor III

Attached is the minimum code to show the spurious NULL character.   Screen capture of terminal program is also attached.

I am using FRDM-KE15Z.   The same problem can also be reproduced in FRDM-KE16Z, or an KL27 target.

To build the program, import KE15Z helloworld example.  Remove all folders except CMSIS, device, startup.  Also remove all files in Source folder.   Copy attached file into Source folder.   Then it should build.

FRDM is already connected with microUSB cable since you are building and downloading the project.  To test the program, open a Terminal program.   Set to 115200-8-1.

  • Debug/run the project.   Any character typed on Terminal will be echoed, except the marker char '%'.
  • Disconnect and reconnect USB cable to cycle power of FRDM board.
  • Reconnect COM port in Terminal program.
  • Enter '%' character and you will get "X 0106".   X represents the NULL received.   Count of 0x0106 = 262 ~= 87 uSec @ 3MHz clock.

Note: P&E Micro Probe appears to have the same problem.

0 件の賞賛
返信
3 返答(返信)

3,571件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Jei,

Hope you are doing well. Are you able to reproduce the same results using the examples we provide for the UART interface?

This is interesting, since we do not define the PCR -PE or PS mask in our examples either. Could you please describe what you are connecting to your UART. Are the voltage levels on the TX and RX line low or high when starting the for(;;) loop?

Best Regards,

Sabina

0 件の賞賛
返信

3,571件の閲覧回数
madisonchou
Contributor III

Further dig using scope.   The spurious NULL received is caused by the floating Rx line.

Guess the correct way of initializing UART is to pull-up the port.   Add these two instructions seem to resolve the problem:

PORTC->PCR[ 6 ] |= PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;
PORTC->PCR[ 7 ] |= PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;

0 件の賞賛
返信

3,571件の閲覧回数
madisonchou
Contributor III

Note: Further test seems to show, not the probe, but the LPUART module in KE15 self-generated a NULL ~87uSec after power-up.

0 件の賞賛
返信