MCU(K10) reset although watchdog is feed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCU(K10) reset although watchdog is feed

跳至解决方案
3,841 次查看
yanlicheng
Contributor III

I develop a project on the K10 chip and use the software watchdog to detect 'system running', and then I met with the following strange issue:

I feed the wdog periodically, but the MCU still reset after running for a short time.

Watchdog is set as follows, can anyone check if it's right :

static void wdog_unlock(void)
{
DisableInterrupts;
WDOG_UNLOCK = 0xC520;
WDOG_UNLOCK = 0xD928;
EnableInterrupts;
}


void wdog_init(void)
{
wdog_unlock();
WDOG_PRESC = 0x0400;
WDOG_TOVALH = 0x01c9; /*timer out is 3s*/
WDOG_TOVALL = 0xc380;
WDOG_STCTRLH = 0x01D3;
}


void wdog_feed(void)
{
wdog_unlock();

WDOG_PRESC = 0x0400;
WDOG_REFRESH = 0xA602;
WDOG_REFRESH = 0xB480;
}

The place I feed the watchdog is:

void pvPollingThread()

{

            if( eMBPoll(  ) != MB_ENOERR )       

                 break;

            wdog_feed();

}

It's a polling thread, and every 2 seconds,  the MCU will receive a message, then go handle the event (cost about 100 milli seconds). Otherwise, it'll go into the next loop.

I use oscillograph to detect the wdog_feed frequency. When no events need to be handled,  the wdog is feed after several microseconds; when event occurs, the wdog is feed after several milli-seconds. Thus, wdog is not feed at a fixed frequency( first short interval ,then long interval, but all within 1s, less than the required 3s ).  Does it matter?

When no events need to be handled, the wdog is always feed at a high frequency, the MCU won't reset.

标签 (1)
标记 (1)
1 解答
3,503 次查看
mjbcswitzerland
Specialist V

Hi

The watchdog feed sequence should be:

DisableInterrupts;

WDOG_REFRESH = 0xA602;

WDOG_REFRESH = 0xB480;

EnableInterrupts;

Regards

Mark

在原帖中查看解决方案

11 回复数
3,504 次查看
mjbcswitzerland
Specialist V

Hi

The watchdog feed sequence should be:

DisableInterrupts;

WDOG_REFRESH = 0xA602;

WDOG_REFRESH = 0xB480;

EnableInterrupts;

Regards

Mark

3,503 次查看
yanlicheng
Contributor III

Thanks for your reply. You mean that we needn't the "wdog_unlock" process each time we feed the dog?

0 项奖励
回复
3,503 次查看
mjbcswitzerland
Specialist V

Yanli

You ONLY need to use the unlock sequence when writing configuration changes to the wathdog, but you DO need to protect the sequence again interrupts.

pastedImage_1.png

An interrupt occuring between the two refresh writes will require 22 clock cycles to save and restore the stack, or 56 if it has an FPU. Assuming your bus clock is half your core clock, and you don't use a part with FPU, you don't need to disable interrupts as long as you:

- have only one interrupt routine that can ever occur

- this interrupt routine requires less that 18 clock cycles to complete

Otherwise you need it - unless you can accept your product having a high probability of resetting each time you service its watchdog (as you already have seen).

Regards

Mark

3,503 次查看
yanlicheng
Contributor III

Hi, Mark:

From your explanation, you mean that:

(1)  "feed the watchdog" doesn't  belong  to  "writing configuration changes to the watchdog", so I needn't do the 'unlock' process.

(2) When I "feed the watchdog" (write 2 different values to WDOG Refresh Register),  interrupt will produce and cost more than "20 bus clock". So I need "DisableInterrupts" first. The feed dog sequence should be as you mentioned above,

DisableInterrupts;

WDOG_REFRESH = 0xA602;

WDOG_REFRESH = 0xB480;

EnableInterrupts;

Am I right? I'll try your method next Monday. Thanks a lot for your answer.

Regards

Yanli

0 项奖励
回复
3,503 次查看
mjbcswitzerland
Specialist V

Yanli

Yes, correct.

Regards

Mark

0 项奖励
回复
3,503 次查看
yanlicheng
Contributor III

Thanks very much, Mark.

I tried your method, and it did work. The MCU doesn't reset any more.

But I'm still confused about one point: Why my old "watchdog feed" method work right in the old project (in which wdog was fed at a regular frequency about 0.5s) ?

According to your explanation ,the old way to feed the wdog should always end with "MCU reset".

I'd appreciate your further explanation.

Regards,

Yanli

0 项奖励
回复
3,503 次查看
mjbcswitzerland
Specialist V

Yanli

In your other project you must have been lucky that there were never interrupts occurring during the watchdog feed - otherwise it would certainly have reset too...

Regards

Mark

0 项奖励
回复
3,503 次查看
yanlicheng
Contributor III

Got it, thanks.

0 项奖励
回复
3,503 次查看
santiago_gonzal
NXP Employee
NXP Employee

Hello Mark,

Where did you get those values from? All the RM and source code I've checked uses the values mentioned by Yanli Cheng.

Regards,

Santiago

0 项奖励
回复
3,503 次查看
mjbcswitzerland
Specialist V

Santiago

I just copied/pasted Yanli's values:

pastedImage_0.png

Did you mix this with the unlock sequence?

Regards

Mark

3,503 次查看
yanlicheng
Contributor III

Thanks! Hopes for more discussion from you about this issue, because I have a limited knowledge about 'watchdog' module.

0 项奖励
回复