Hi,
I read the MCG chapter in KL26 reference manual, found a MCGFFCLK clock, but I cannot find where it is in the Clocking diagram.
The sentence is "The MCG Fixed Frequency Clock (MCGFFCLK) provides a fixed frequency clock
source for other on-chip peripherals; see the block diagram."
But nothing is about the block diagram.
Thanks,
Henry Xin
Hi, Henry Xin
For Kl25, Pls refer to the section 5.3 High-Level device clocking diagram, especially Figure 5-1. Clocking diagram, I do not think the KL25 has defined the MCGFFCLK clock source, none of peripheral uses the MCGFFCLK clock.
BR
XiangJun Rong