MAXIMUM FLASH CYCLES IN KEA-128 FOR WEARING OUT???

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MAXIMUM FLASH CYCLES IN KEA-128 FOR WEARING OUT???

1,670件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

     what is the Maximum Flash cycles KEA-128 controller can withstand and will not wear out?

3 返答(返信)

1,473件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNE SH BALAJI,

From the KEA128 datasheet, you can get that the Flash Program/erase endurance is typically 100K Cycles, the max data is not gave out, we also don't have it.
Flash have the lifetime, it is the character of the flash.
So, when you evaluate this chip's flash cycle, please use the typical data, this data is guaranteed.
About the document, please refer to this link:
http://www.nxp.com/assets/documents/data/en/data-sheets/S9KEA128P80M48SF0.pdf


Page 22.

Wish it helps you!
If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,473件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Kerry,

              Can you help me in Getting the max data for Flash Program/erase endurance? Also can you say under what conditions the Flash Program/erase endurance test was taken??? 

0 件の賞賛
返信

1,473件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

HI Vignesh

There is not max spec.

please check this old document as reference for the typical endurance EB619

Regards

Vicente