MAC Address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MAC Address

3,004 次查看
razumovskyeduar
Contributor I

Hi

Does K64 comes with MAC address ? Should it ?
If so, is it a default MAC address or unique ?
Do i need to buy MAC address and configure it in the production ?

Thanks

0 项奖励
回复
2 回复数

2,432 次查看
bobpaddock
Senior Contributor IV

Microchip sells several EEPROMs that come with MAC addresses that can be copied into the K64 on boot.

Unless making a lot of a widget it is usually cheaper to go this route than buying the IEEE addresses.

Mark's link explains the process.

MAC Address Chips Products - Microchip Technology Inc 

0 项奖励
回复

2,432 次查看
mjbcswitzerland
Specialist V

Hi

The K64 has no MAC address programmed in it anywhere as delivered.

See the following for details of purchasing MAC addresses for your products: http://www.utasker.com/forum/index.php?topic=21.msg67#msg67

It is the responsibility of the manufacturer of the product (yourself) to program unique MAC addresses to each device from the allocated range - a good method is to save these in the PROGRAM ONCE area of the K64's Flash so that it can never be modified.

Regards

Mark

Kinetis for professionals: http://http://www.utasker.com/kinetis.html

0 项奖励
回复