Loss of Clock reset when waking from stop mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Loss of Clock reset when waking from stop mode

1,033 Views
dereksnell
NXP Employee
NXP Employee

I wanted to point this out after working on an issue.  The snippet from the reference manual below shows the MCG clock monitor needs to be disabled when entering any stop mode, VLPR, or VLPW.  This is done by clearing the CME bit in MCG_C6.  If CME is set when entering a low power mode, it can cause resets.  As of MQX v3.8.1, some BSPs do have the CME bit set when entering a low power mode.  This issue has already been reported to the MQX team.

Snippet.jpg

0 Kudos
Reply
0 Replies