Looking for a quick bootloader solution and much, much more? For me it was uTasker (K64 family in my case)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for a quick bootloader solution and much, much more? For me it was uTasker (K64 family in my case)

4,025件の閲覧回数
orangeusa
Contributor III

(Not affiliated with uTasker - but Mark has helped in the past with other questions on this forum. )

BOOTLOADER NEEDS:

Yeah, I am a hardware guy, and needed a bootloader yesterday. I have written bootloaders in the past, but they take a lot of time at both the firmware and PC level (Windows/AOS, whatever). They have to be perfect and be able to handle failed application downloads. They are a bugger to debug as you cannot single step through them easily.....

I was stuck with a tight schedule (3 months for 2 board designs, firmware, and programmable logic). Routing, PCB turnaround, purchasing/selecting parts, PCA assembly.... 

My hardware is in routing, will be built in a couple weeks. So firmware was turning out to be my biggest risk - especially the bootloader.

uTASKER BOOTLOADER:

So I started fiddling with uTasker.  Of course I didn't read the manuals, had some dumb self-created issues.  Bottom line - read the manuals, and take care in setting those equates..

BUT - after you take time to understand the USB Demo and other demos, changing a few equates vs. writing 1k lines of code yourself is easy.  I literally changed a few equates in the SerialLoader_Flash config.h file and viola!  The MSD-USB ( looks like a PnP Mass Storage Device on the PC when you boot with SW2 pressed during reset or poweron... ). Perfect for field support or Production support as it's really simple and rugged.

MAIN CODE:

I mostly need a CDC interface - which this has - literally you can have multiple CDC ( virtual COMM ports ) with 1 equate.

Add a few lines of code to parse them and you are in business.

I'm not near finishing my code, but this package saved me months of firmware development and is quite flexible.

Remember - in the case of the K64 processors - the document describing the registers is like 1789 pages. I know because I printed them out. lolz. 4-5" tall. wow.

That's all I have - worked out well for me.

ラベル(3)
1 返信

3,562件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Scott,

Freescale provides some application note about Kinetis K60 product bootloader, you can use these as reference, you could download from below links:

AN4370 USB DFU bootloader http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4370.pdf

AN4368 USB Mass Storage Device Host Bootloader  http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4368.pdf

AN4379 Freescale USB Mass Storage Device Bootloader  http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf?fasp=1&WT_TYPE=Application...

AN4367 Ethernet Bootloader for MCU http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf?fasp=1&WT_TYPE=Application...

Wish it helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------