Linkserver does not program MK70FX512VMJ12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linkserver does not program MK70FX512VMJ12

Jump to solution
1,864 Views
dodocolby
Contributor II

Hello,
I purchased the MCU-LINK-PRO so I can install a bootloader for the MK70FX512VMJ12.
in the product info for the MCU-LINK-PRO is mentioned that is able to program the K70-120 family.
please provide some hints, any help appreciated.

 

 

however, when trying to install I get the following message:

> C:\NXP\LinkServer_25.6.131\LinkServer.exe flash --probe W1BZIZQQLDBOA Generic-M4: load --erase-all C:/Users/320260965/Desktop/MAC_Bootloader.s19 Ns: LinkServer RedlinkMulti Driver v25.6 (Jun 26 2025 19:34:05 - crt_emu_cm_redlink.exe build 1017) Pc: (  0) Reading remote configuration Wc(03). No cache support. Nc: Found generic directory XML file in C:\Users\320260~1\AppData\Local\Temp\tmp82k6tlhx\crt_directory.xml Pc: (  5) Remote configuration complete Nc: Reconnected to existing LinkServer process. Nc: Probe Firmware: MCU-LINK Pro (r0CF) CMSIS-DAP V2.241 (NXP Semiconductors) Nc: Serial Number:  W1BZIZQQLDBOA Nc: VID:PID:  1FC9:0143 Nc: USB Path: \\?\hid#vid_1fc9&pid_0143&mi_00#7&1092ae21&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030} Nc: Using memory from core 0 after searching for a good core Pc: ( 30) Emulator Connected Pc: ( 40) Debug Halt Pc: ( 50) CPU ID Nc: debug interface type      = CoreSight DP (DAP DP ID 2BA01477) over SWD TAP 0 Nc: processor type            = Cortex-M4 (CPU ID 00000C24) on DAP AP 0 Nc: number of h/w breakpoints = 6 Nc: number of flash patches   = 2 Nc: number of h/w watchpoints = 4 Nc: Probe(0): Connected&Reset. DpID: 2BA01477. CpuID: 00000C24. Info: <None> Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled. Ns: Content of CoreSight Debug ROM(s): Nc: RBASE E00FF000: CID B105100D PID 04000BB4C4 ROM (type 0x1) Nc: ROM 1 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0) Nc: ROM 1 E0001000: CID B105E00D PID 04003BB002 Gen DWT (type 0x0) Nc: ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0) Nc: ROM 1 E0000000: CID B105E00D PID 04003BB001 Gen ITM (type 0x0) Nc: ROM 1 E0040000: CID B105900D PID 04000BB9A1 CSt TPIU type 0x11 Trace Sink - TPIU Nc: ROM 1 E0041000: CID B105900D PID 04000BB925 CSt ETM type 0x13 Trace Source - Core Nc: ROM 1 E0042000: CID B105900D PID 04003BB907 CSt ETB type 0x21 Trace Sink - ETB Nc: ROM 1 E0043000: CID B105900D PID 04001BB908 CSt CSTF type 0x12 Trace Link - Trace funnel/router Nc: NXP: Generic-M4 Nc: DAP stride is 4096 bytes (1024 words) Pc: ( 65) Chip Setup Complete Pc: ( 70) License Check Complete Ed:05: File 'tmpuzuinkpe.elf' load failure: Ef(11). No flash configured at the specified address. Pc: (100) Target Operation Failed

 

 

Tags (1)
0 Kudos
Reply
1 Solution
1,756 Views
ErichStyger
Specialist I

It seems the article did not store the file, so I try here again.

I hope it works this time.

Erich

View solution in original post

6 Replies
1,787 Views
ErichStyger
Specialist I

Hi @dodocolby ,

I have created a K70 file for you.

Please unpack the zip file and place the JSON file inside the following folder:

<LinkServerInstallationPath>\devices

If you start now LinkFlash, you should see the K70:

ErichStyger_0-1778241696370.png

I only have the K70FN1M device, and it worked for me:

ErichStyger_1-1778241726054.png

 

Can you try this for your K70FX512 too and report back?

I hope this helps,

Erich

0 Kudos
Reply
1,773 Views
dodocolby
Contributor II
Thank you Mr Erich Styger,
is there a link for the json file?
0 Kudos
Reply
1,757 Views
ErichStyger
Specialist I

It seems the article did not store the file, so I try here again.

I hope it works this time.

Erich

1,843 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @dodocolby 

Please refer to the MCU-LINK PRO User Manual, section 3.2 “Updating MCU-Link Pro Firmware”, and update the firmware accordingly. I  recommend you update it to j-link firmware.

If the issue still persists, please provide a video or screenshots showing your steps. I will help check and analyze the issue.

Thank you.

 

BR

Alice

0 Kudos
Reply
1,820 Views
dodocolby
Contributor II

Hello,
I ran the program_CMSIS.cmd from the scripts of MCU-LINK_installer_3.172.
(running the program_JLINK.cmd results in the device not appear as probe in linkserver).

Then I run linkflash.exe that calls linkserver version v26.3.123.
K70 is not enumerated (no device has k70 in their name).
I choose Protocol SWD, Nothing for Wirespeed, the same "Generic arm-4:" as device I ran into the same problem:


> C:\NXP\LinkServer_26.3.123\LinkServer.exe flash --probe W1BZIZQQLDBOA Generic-M4: load --erase-all C:/Users/320280032/Documents/Projects/0Docs_Windchill/Gen4/Processor/Programmers/MAC_Bootloader.s19

...


Nc: NXP: Generic-M4
Nc: DAP stride is 4096 bytes (1024 words)
Pc: ( 65) Chip Setup Complete
Pc: ( 70) License Check Complete
Ed:05: File 'tmpy31vs5hc.elf' load failure: Ef(11). No flash configured at the specified address.
Pc: (100) Target Operation Failed

However, I chose another device that seems to have similar characteristics to the MK70 I have:  MK64FX512xxx12:FRDM-K64F instead of MK70FX512VMJ12. That programming resulted in success:

Nc: Sectors written: 20, unchanged: 0, total: 20
Nc: Closing flash driver FTFE_4K.cfx
Pb: (100) Finished writing Flash successfully.
Nt: Loaded 0x13424 bytes in 874ms (about 90kB/s)
Nt: Reset target (system)
Nc: Starting execution using system reset




The big question now is if that is ok to choose the other device, because MK64 is a different family than MK70?

 

 

0 Kudos
Reply
1,793 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @dodocolby 

 

Thanks for your reply.

I have checked LinkFlash, and it does not support the MK70. If the flash size and address are identical between the MK64 and MK70, using the MK64 might be an option to try.

However, a more reliable method is to use J-link firmware on MCU-link.

run program_JLINK.md under
LinkServer_25.6.131\MCU-LINK_installer\scripts
to update the MCU‑Link firmware to J‑Link, and then use the J‑Flash tool to connect to the K70 and program it.

Alice_Yang_0-1778227305204.png

 

 

Thank you.

 

BR

Alice

0 Kudos
Reply