LWIP IPV6 example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LWIP IPV6 example

3,002件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I am trying the double stack option with LWIP. The local link address is replying to the ping. 

I try to add the lines

IP6_ADDR(ip_2_ip6(&(fsl_netif0.ip6_addr[1])), 0xc30600fc, 0x91a853c3, 0x0, 0x04000000 );
IP_SET_TYPE_VAL(fsl_netif0.ip6_addr[1], IPADDR_TYPE_V6);

I suppose the address will be added to the auto configured. 

The ping

ping -6 fc00:6c3:c353:a891::4  

does not get a reply. Is there something wrong in the added lines for setting the pinged address, or I should do more than this....

Help needed..

Thank You

Pietro

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)