LPUART Transmitter Active Soon as Enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPUART Transmitter Active Soon as Enabled

Jump to solution
1,388 Views
Mike_d
Contributor IV

Hi,

I trying to figure out why the TC status shows it as sending data the line after the transmitter is enabled and never goes idle.

Regards,

-Mike

0 Kudos
Reply
1 Solution
1,207 Views
Mike_d
Contributor IV

Found it.  I didn't have the PLL selected.

SIM_SOPT2 |= SIM_SOPT2_PLLFLLSEL(1);

View solution in original post

0 Kudos
Reply
3 Replies
1,208 Views
Mike_d
Contributor IV

Found it.  I didn't have the PLL selected.

SIM_SOPT2 |= SIM_SOPT2_PLLFLLSEL(1);

0 Kudos
Reply
1,207 Views
Mike_d
Contributor IV

So which is correct?  My problem is the TC bit is always 0.

pastedImage_2.png

pastedImage_3.png

0 Kudos
Reply
1,207 Views
mjbcswitzerland
Specialist V

Mike

pastedImage_1.png

The default for this flag is to be set, meaning that it will interrupt immediately when the UART is enabled if its interrupt mask is set.
It only goes to '0' while transmission is taking place and is set back to '1' (can generate interrupt) when the transmission terminates (idle-line again).
This is the same behavior as the TDRE flag apart from the fact that the TDRE goes high again when the data has been shifted out rather than after the last bit period has terminated.

Regards

Mark
Kinetis for professionals: http://www.utasker.com/kinetis.html

0 Kudos
Reply