LPSPI + DMA Buffer start from 4th index for slave device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI + DMA Buffer start from 4th index for slave device

6,774 Views
Sridharanblr
Contributor I

Hi ,

We are using the MKE15Z256xxx7 controller for transfer and receive the data through SPI with DMA for Pmod-sf3 flash( Customized SPI driver) . The communication is fine, Read/Write too is also fine, however the data is read from index 4 instead of 0th index, ie first we need this data to be from 1st index. 

E.g : Current working of code 

Write command : Buffer status 

WriteBuff[10u] = {0x02, 0x00, 0xff, 0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06};
ReadBuff[10u] = {0xff, 0xff, 0xff, 0xff, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};

Read Command:  Buffer status 

WriteBuff[10u] = {0x03, 0x00, 0xff, 0x00, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff};
ReadBuff[10u] = {0xff, 0xff, 0xff, 0xff, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06};

 

Expected: Read command: Should read from index 0. 

WriteBuff[10u] = {0x03, 0x00, 0xff, 0x00, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff};
ReadBuff[6u] = {0x01, 0x02, 0x03, 0x04, 0x05, 0x06};

 

Here we are using a single buffer which contain Command + Address + Data, We are using same buffer for writing and while reading too. 

Query : 

1. We wanted the data to be read from 0th index.

2. Can we have a sample code SDK (SPI + DMA) which uses separate buffer for command/Address and read/write.

3. How can we not trigger the interrupt for first 4bytes( Command+Adress) and then trigger SPI interrupt so that it read from 0th index. 

 

 

 

 

 

 

 

Labels (1)
0 Kudos
Reply
10 Replies

6,680 Views
Sridharanblr
Contributor I

Hi Raul,

the above screenshot and our reply is based on  MKE15Z256 SDK  frdm15z_lpspi_edma_b2b_transfer_master. 

jfi: Without DMA we first written the Command and address to TDR register and then we enabled SPI interrupt, by this way the read/Write was exactly happing for 1st index location of the buffer. 

0 Kudos
Reply

6,643 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Sridharanblr,

Just for double check could you please confirm if the signal screen shot was using eDMA?

Also, could you try writing the Command (0x03) + address (0x00 0xFF 0x00) to TDR register before enabling the EDMA_EnableChannelInterrupts, to see if you can replicate the reading/writing in 1st index in SPI with the eDMA?

Best regards, Raul.

0 Kudos
Reply

6,627 Views
madhavaishriram
Contributor II

Hi @RaRo 

We have tested with by writing Cmd 0x03 and Address 0x00, 0xff, 0x00 in to TDR register.

but getting same issue after that too.

Please find the code before read.

madhavaishriram_0-1672985325882.png

 

Below is the code to writing into TDR register directly.

madhavaishriram_1-1672985465421.png

 

The snap after read by calling read api.

madhavaishriram_2-1672985539203.png

 

Please see the log after read.

madhavaishriram_3-1672985577817.png

 

0 Kudos
Reply

6,589 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @madhavaishriram,

Could you please check if this behavior still happens using the LPSPI+eDMA communication with another device?

Regards, Raul.

0 Kudos
Reply

6,534 Views
madhavaishriram
Contributor II

HI @RaRo 

We have PMOD-SF3 as slave device and tested on same device and getting same behavior with and w/o dma. So please check at your end and reply with solutions,

 

Thanks and Regards,

Shriram Madhavai

 

 

0 Kudos
Reply

6,520 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @madhavaishriram,

Unfortunately, we don't have a PMOD-SF3 flash to replicate your issue. We recommended you the example code, because the reading of data should work from the first index.

As a suggestion, you could try reading/entering another direction of the flash.

Also, looking at 3V, 256Mb: Multiple I/O Serial Flash Memory PMOD-SF3 datasheet (Command Definitions [Table 18. Command Set]), for writing/programming data in the flash you first need to enable the writing; just for double check, you could confirm if you are enabling the writing first before programming the data to the flash and disabling it before reading the data [WRITE Operations].

Finally, you could try using only SPI first to see if everything it is working fine, before trying out with DMA.

Best regards, Raul.

0 Kudos
Reply

6,731 Views
Sridharanblr
Contributor I

Hi @RaRo 

Yes, we did same changes in SDK we found same behaviors, The read data is from 4th index. 

Below changes was reworked on SDK : 

 Master : NXP FRDM HW

Slave : PMOD SF3 

Write command/Address/Data(250) : 0x2, 0x00, 0xff,0x00, xx,xxx,xxx........upto 250byte

Read command/Address/Data(250) : 0x3, 0x00, 0xff,0x00, Data reading starts from here ie 4th index. 

Sridharanblr_1-1672297014584.png

 

Regards

Sridharan 

 

0 Kudos
Reply

6,726 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Sridharanblr,

Could you please try out with other examples that don't include eDMA? For example, lpspi_interrupt_b2b_transfer_master and/or lpspi_polling_b2b_transfer_master. This way we could see if it is something to do with the eDMA and how it handles the data and the buffer.

Also, could you please attach the signal behavior with a logic analyzer of the transfer?

Regards, Raul.

0 Kudos
Reply

6,717 Views
madhavaishriram
Contributor II

Hi @RaRo 

Please find the attached snap for without DMA transmission with PMOD-SF3 and the logic analyzer data.

We have seen same issue.

madhavaishriram_0-1672376941662.png

madhavaishriram_1-1672377204815.png

 

Regards,

Shriram Madhavai

Tags (1)
0 Kudos
Reply

6,743 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Sridharanblr, 

Just for double check, could you please try out the MKE15Z256 SDK examples: frdm15z_lpspi_3wire_edma_transfer_master and frdm15z_lpspi_edma_b2b_transfer_master?

Are you seeing the same issue with the examples?

Regards, Raul.

0 Kudos
Reply