LOCKUP reset ( USB )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LOCKUP reset ( USB )

Jump to solution
2,896 Views
CCandido
Contributor V

Hi,

project example usb for MKS22.

Reset or  HardFault_Handler ( LOCKUP bit ).

my board power usb = 3.3v, cap-47uF, cap-100k, usb_cable short.

my test:

pullup resistor on RESET_PIN = 10K, 4K7, 1K, 100r ( ERROR).

else:

pullup resistor on RESET_PIN = 27R = ( ok )

exites other solution ?

thanks,

Carlos.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,703 Views
CCandido
Contributor V

Hi Jing

I tested solution register RST, not solution,

I tested ( add, Capacitor 10uF and 100nF ) on Pin VDDUSB = ok, running, not more problems LOCKUP.

thanks,

Carlos.

View solution in original post

0 Kudos
Reply
3 Replies
2,703 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

"The RESET_b pin, if enabled, must have a 100 nF capacitor close to the MCU for transient protection. The NMI_b pin, if enabled, must not have any capacitance connected to it. Each pin, when enabled as their default function, has a weak internal pullup, but an external 4.7 kΩ to 10 kΩ pullup is recommended. As with power pin filtering, it is recommended to minimize the ground loop for the capacitor and the VDD loop for the pullup resistor for these pins.
The RESET_b pin also has a configurable digital filter to reject potential noise on this input after power-up. The configuration bits are located in the RCM_RPFC register. While use of this filter may negate the need for the pullup and capacitor mentioned above, it is still recommended to use external filtering in electrically noisy environments."

Other hardware and software setting details please find in KQRUG.pdf with can be found in www.nxp.com.

Regards,

Jing

0 Kudos
Reply
2,704 Views
CCandido
Contributor V

Hi Jing

I tested solution register RST, not solution,

I tested ( add, Capacitor 10uF and 100nF ) on Pin VDDUSB = ok, running, not more problems LOCKUP.

thanks,

Carlos.

0 Kudos
Reply
2,703 Views
CCandido
Contributor V

Hi Jing,

I will do tests.

has a strange fact, when I call (serial debug or programmer) it slows down USB CDC errors,

slow down also the resets.

thanks.

Carlos.

0 Kudos
Reply